2019-11-26 6:28 AM
I got two these STM32H750 boards. Wired up a ST-LINK, and one of them works fine.
But the second one is not accessible by debugger.
Following is output of CubeIDE debugger:
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on targetAnd this is output of CubeProgrammer:
STM32CubeProgrammer API v2.1.0
ST-LINK SN : xxxxxxxxxxxxxxxxxxx
ST-LINK FW : V2J34S7
Voltage : 1.57V
Error: ST-LINK error (DEV_TARGET_CMD_ERR)
ST-LINK SN : xxxxxxxxxxxxxxxxxxxxxx
ST-LINK FW : V2J34S7
Voltage : 0.55V
Error: ST-LINK error (DEV_TARGET_CMD_ERR)
ST-LINK SN : xxxxxxxxxxxxxxxxx
ST-LINK FW : V2J34S7
Voltage : 0.00V
Error: No STM32 target found!The board is alive, it runs some pre-installed firmware that blinks the LEDs. Looks exactly as the other (good) one.
Can it be a symptom of level 2 activated, or the new STM32H75x "secure mode"?
Thanks,
-- pa
Solved! Go to Solution.
2019-11-26 12:25 PM
Voltage seems very low. Check connection soldering and continuity of both VCC and GND.
2019-11-26 11:26 AM
Have you tried mass erase?
2019-11-26 12:09 PM
I don't have direct H7 experience,m but on other STM32 families, when RDP2 (or RDP1) protection is set the ST-Link will still connect and "see" the device, it just won't let you do much. Since you are seeing "no device found" I would suspect the SWI interface. Though looking at the schematic from the other thread there isn't anything there except header/connector and CPU. Double-check the solder joints???
2019-11-26 12:25 PM
Voltage seems very low. Check connection soldering and continuity of both VCC and GND.
2019-11-26 4:52 PM
> Have you tried mass erase?
No. Cannot connect with any tool: programmer, ST-LINK utility.
2019-11-27 1:56 AM
Yep. Soldering it was ((
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.