2019-11-21 11:35 PM
Hi All
I am just starting off with the STM parts and bought the 469 EVM. I got the touch ID with TouchGFX working and made some cool things but now it is time to start using the periphials on the board in bare metal C config.
I am really looking to do simple things like the joystick, ADC, Uart etc for now. Are there any resources or sample code for getting each of the things on the board up and running so you can build up from there?
Can i get some pointers to resources that would assist please. Just something like reading the ADC and sending out the serial would be good, and using the joystick to switch the LEDS. Simple things like that.
Did anyone else have a problem where the cubeIDE code for the EVM wouldn't get past the MMC init function. I had to comment it out to get past it.
Thanks in advance.
2019-11-22 1:53 AM
F769I or F469
Should be a whole bunch of board level peripheral examples in the CubeF7 repository as unpacked.
2019-11-26 5:06 PM
F469!
Where do i locate the CubeF4 repository of board level examples?
2019-11-26 6:51 PM
Where did you install it via CubeMX / CubeIDE ?
Here's the archive
https://www.st.com/en/embedded-software/stm32cubef4.html
STM32Cube_FW_F4_V1.24.1\Projects\STM32469I_EVAL\Examples\BSP
STM32Cube_FW_F4_V1.24.1\Projects\STM32469I_EVAL\Applications\Display\LCD_PicturesFromSDCard
STM32Cube_FW_F4_V1.24.1\Projects\STM32469I_EVAL\Demonstrations\TouchGFX
STM32Cube_FW_F4_V1.24.1\Drivers\BSP\STM32469I_EVAL\stm32469i_eval.c
2019-11-26 10:40 PM
Thank you. Great. BTW. If i wanted to find a contractor here on the community to create a BSP based upon the 469 EVM suited to my requirements, on FreeRtos - where would i go to find such a person to handle it to jump start me ahead on to my main application code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.