STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Disable nterrupt inside the IRQ Handler allowed??

Hello,i disable the interuppt after its execution is it allowed?void EXTI4_IRQHandler(void) { // Clear interrupt __HAL_GPIO_EXTI_CLEAR_IT(SYNC_UC_PIN);   // call function function();// the function enables an other interrupt of the same pri...

Jannaros by Associate II
  • 3541 Views
  • 7 replies
  • 0 kudos

STM32L010 FLASH_SR bit OPTVERR set when erasing a flash page

I am using an STM32L010k8 with HAL driver version 1.11.2, when I erase a single flash page at address 0x08004000, the very first call to function FLASH_WaitForLastOperation within HAL_FLASHEx_Erase fails because the OPTVERR bit in FLASH_SR register i...

SThom.7 by Associate III
  • 864 Views
  • 0 replies
  • 0 kudos

OpenOCD failed : stm32f4x.cfg:77: Error: invalid subcommand "newtap stm32f412 cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0x4ba00477"

Hi experts,We have created a project on WICED 43xx_Wi-Fi sdk for STM32F412 MCU+43438 wlan chip.We have connected st-link V2 debugger to the EVB and we could see "STM32 STLink"​ in windows Device Manager.When we used openOCD to flash debugger to EVB, ...

STM32F769NI Evaluation board NEWBIE

Hi AllI am just starting off with the STM parts and bought the 469 EVM. I got the touch ID with TouchGFX working and made some cool things but now it is time to start using the periphials on the board in bare metal C config.I am really looking to do ...

Can I use the Quad SPI memory controller peripheral on STM32F4xx series to access a PSRAM or SRAM IC rather than a flash IC, and have the data memory map as if internal RAM?

I am hoping to use the CMSIS/DSP libraries to work on data that I periodically store on external RAM. If it is important, my current plan is to use the Lyontek LY68L6400 PSRAM or the VTI7064 SRAM (more expensive). Both are 64Mb volatile memory ICs th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.