2018-03-22 10:54 AM
Hello!
I have just updated CubeMX to 4.25.0 but none of the generated codes work within Keil. If i use code from older projects which were made by CubeMX 4.24 ,they work flawlessly but if i generate a simple initialization code with CubeMX and try even blink a LED on STM32L476 Discovery board it does not work.
Did anyone notice some troubles with the update?
int main(void)
{ /* USER CODE BEGIN 1 *//* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_I2C1_Init(); MX_I2C2_Init(); MX_LCD_Init(); MX_QUADSPI_Init(); MX_SAI1_Init(); MX_SPI2_Init(); MX_USART2_UART_Init(); MX_USB_HOST_Init(); /* USER CODE BEGIN 2 *//* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { HAL_Delay(300); HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_2);/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */}
2018-03-30 10:51 PM
If you are using PLL, it's probably it's missing
RCC_OscInitStruct.PLL.
PLLM inSystemClock_Config().
2018-04-25 7:39 AM
Hi Istvan,
Thanks for your feedback and sorry for late response.
To figure out this issue, can you please specify your:
Keil version.
STM32Cube FW_L4 version.
Additionally, it will be more helpful if you share your CubeMX project (.ioc)
Thanks in advance for helping to complete this thread.
Best Regards,
Mohamed
2018-09-16 10:26 PM
I have the same problem..
CubeMX 4.26.1(STM32Cube_FW_L1_V1.8.1) + STM32L152CDISCO board
MX_LCD_Init()
HAL_StatusTypeDef HAL_LCD_Init(LCD_HandleTypeDef *hlcd)
.
.
.
/*!< Wait Until the LCD Booster is ready */
while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > LCD_TIMEOUT_VALUE)
{
hlcd->ErrorCode = HAL_LCD_ERROR_RDY;
return HAL_TIMEOUT;
}
}
HAL_TIMEOUT error!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.