Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on March 22, 2018 at 18:54Hello!I have just updated CubeMX to 4.25.0 but none of the generated codes work within Keil. If i use code from older projects which were made by CubeMX 4.24 ,they work flawlessly but if i generate a simple initializ...
Hi,I found many bugs in the given application example like1) Wrong clock configuration, which lead to hard fault error 2) Wrong ports configuration, which is not enabling USB Host port powerand many more unknown due to which HID keyboard is not commu...
Using STM32H743VIT. Plane to use a RGB666 640x480x3 TFT. Configurating IOs using CubeMX version 4.27.0. First of all, when expanding LTDC pheripheral I only find two out of 8 possible modes, i.e. RGB666 and RGB 565. The RGB888 and ARGB' variants etc....
Hello everybody,I read everything I found, and it's still not clear.First, I've got my OTG_FS_Core in OTG mode with ID line.I don't need High Speed USB.Q1: Is there 2 dedicated FS Phy, (one for each Core, FS and HS)?Q2: How can I get the OTG_HS_Core ...
I attached a battery to my STM32, and my RTC is now keeping the time when the board is not powered.But when not powered, the clock is also not advancing, which means that when I power on the board, the RTC shoes the time when I powered off the board....
I've an STM32F103C8T6 CPU, but I can't find appropriate linker file. The closes file is `STM32F101XB_FLASH.ld`. Can I use it with change following line (#43):FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 128KtoFLASH (rx) : ORIGIN = 0x08000000,...
I'm trying to convert 3 ADC channels using DMA. But the variables don't seem to change when I watch them in the debugger. I know the conversion complete callback is executed because I breakpointed it. So this suggests that the DMA transfer is not exe...
Posted on April 13, 2018 at 01:38I have built a custom STM32F446ZE board and I used the ST890CDR current protector and the LD39050PU33R voltage regulator in exactly the same way they are implemented in the Nucleo Board from ST. The only difference i...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.