2025-01-07 2:38 PM
We need to continuously DMA a single 16-bit word to the SPI transmitter. (Neither the memory address nor the peripheral address would increment.) Can this be done without intervention? I.e. do we have to use a DMA Complete interrupt to set a flag and call HAL_SPI_Transmit_DMA whenever the flag gets set, or can we configure HAL_SPI_Transmit_DMA to set and forget it?
2025-01-08 11:47 AM
Here's the relevant code:
MX_SPI2_Init
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi2.Init.NSS = SPI_NSS_HARD_OUTPUT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
HAL_SPI_MspInit
/**SPI2 GPIO Configuration
PC1 ------> SPI2_MOSI
PB10 ------> SPI2_SCK
PB12 ------> SPI2_NSS
*/
GPIO_InitStruct.Pin = SPI2_MOSI;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF3_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
// Remove SPI2_NSS_Pin
GPIO_InitStruct.Pin = SPI2_CLK|SPI2_NSS;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
Main
HAL_StatusTypeDef status = HAL_SPI_Transmit_IT(&hspi2, (uint8_t *)&buf, 1);
2025-01-08 11:55 AM
2025-01-08 12:47 PM
> hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
NSSP only works with CPHA=0, so change this to SPI_PHASE_1EDGE.
2025-01-08 1:05 PM
2025-01-08 1:49 PM
What line do you want to invert? Probably needs to be done in hardware.
2025-01-08 2:02 PM
NSS
2025-01-08 4:03 PM
I don't think the STM32L4 can change the polarity of NSS internally.
The STM32H7 series (and probably other newer chips) can:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.