STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! is it possible to log data in internal flash?

Hii everyone,I am facing the problem for the data logging in flash.i am not able to keep track of the variable till where the flash memory is filled is there any way to sort out this problem. i am not able to erase the single word to update the addre...

Resolved! USB on STM32G0

I developed a user device with a STM32G030 in it. Now I want to go to the market. But before that, I want to have a USB port on my board with which users can update their firmware in case my software has bugs. In the STM32G0x0 datasheet (RM0454) in c...

JanAtze by Associate II
  • 4447 Views
  • 4 replies
  • 1 kudos

nucleu-h745zi-q rs485 without external module

Hello//   nucleu-h745zi-qI want to use hardware flow control rs485Previously, i used an external module because there was only rs232 (f103).** question ** . With this feature, can the module be removed and the microcontroller directly connected to A ...

MGH745 by Associate II
  • 2098 Views
  • 4 replies
  • 1 kudos

Resolved! Why does LwIP need CPU DCache (on STM32H743)?

To enable LwIP in CubeMX (inside CubeIDE) it needs the CPU data cache enabled.  Ok, no problems, but it doesn't explain why and I can't find why this is the case. Is anyone able to offer an explaination?  

musmuris by Associate II
  • 6314 Views
  • 9 replies
  • 3 kudos

How do I set the NUCLEO-L476 to Low power mode

I need to use the energy collection mode of ST25 to wake up L4. The software used now is En.X-Cub-NFC7. How can I modify the example code to set L4 to low power mode and wake up L4 only through the energy of ST25?

Resolved! Uart receiver pb

 i have established communication with a BLDC (Brushless DC) controller. Initially, i send a message to the controller using the function void sendParameter(uint8_t parameter). Following this transmission, the BLDC controller is expected to respond w...

kkhli.1 by Associate III
  • 22325 Views
  • 26 replies
  • 11 kudos

Resolved! NUCLEO-144 H723ZG "Can not connect to the target!"

Hi there,I received a new out of the box NUCLEO-144 H723ZG board which I can not connect, but getting the "Can not connect to the target!" message (see below)What I've done so far:- checked the Jumper as described in user manual UM2407 section 5 >> a...

PGrif.2 by Associate III
  • 4035 Views
  • 7 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.