STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader code for safety device

Hi ST,We are making product targeting SIL3 safety by using STL library. So, I have few doubts :-1. Is it recommended to have a bootloader in a safety grade product?2. If Yes, then how can I proceed? 3. In normal way bootloader code should be written ...

dat mismatch when reading .bin file in stm32 for FOTA

Hi, I want to implement FOTA in stm32, for that I am reading .bin file and send to the controller through UART. And Write that file to the flash memory, All Ihave done this, but there mismatch data beetween .bin file data written on flash.the readi...

ykn by Senior
  • 2027 Views
  • 3 replies
  • 0 kudos

STM32H743 vs STM32H753

I have just started a project and am using the STM32H743. Is there any reason I should switch to the STM32H753? I know they are pin compatible and the 753 has some more advanced crypto features, but I'm more concerned with availability of these parts...

GilRoss by Associate II
  • 3348 Views
  • 3 replies
  • 3 kudos

work out poly

Need a help to work out the formula. I cant get my head around with this to work out. its polynomial with numerator and denominator. what is the formula for this. Thank you FLOAT_TYPE num_coeff[] = {-2.42580348918581e2l, 4.43575581447635e2l, -8.65706...

cjaya.2 by Associate II
  • 2099 Views
  • 5 replies
  • 0 kudos

Resolved! F4 I2S cannot resync after noise

I've got the I2S working with DMA as slave receiver, works great, bit perfectly fills receiving buffer,until I restart the master, or introduce noise to I2S bus, then it just loses it, fills buffer with nonsense after that.It's not able to resync to ...

mrx23 by Associate III
  • 2827 Views
  • 4 replies
  • 0 kudos

How supply STM32F446RET6

Hi, I want to design a board using STM32F446RET6 MCU. But I have a question about how to properly power the ADC system, and what the VCap_1 pin is. I read that I need to put a 4.7 uF ceramic capacitor with low ESR there. Below is an introductory grap...

f446_power.png
MSzła.1 by Associate III
  • 4891 Views
  • 7 replies
  • 1 kudos

Resolved! Migrate from STM32G431CBU6 to STM32G474CCU6

Hi,We are planning migrate our product based on STM32G431CBU6 to STM32G474CCU6. Need to make sure they are compatible in hardware design, are the two pin-to-pin compatible?Thanks. 

Resolved! Wich eval board mcu stm32

Wich eval board mcu stm32 recommend me to learn and in the future can match with dsp.Regards 

Ponch by Associate II
  • 3358 Views
  • 7 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.