2022-10-11 5:06 AM
Hi, I want to implement FOTA in stm32, for that I am reading .bin file and send to the controller through UART. And Write that file to the flash memory,
All Ihave done this, but there mismatch data beetween .bin file data written on flash.
the reading and sending . bin file have done this using GCC compiler.
below the function code.
int main(int argc, char *argv[])
{
int comport;
int bdrate = 115200; /* 115200 baud */
char mode[]={'8','N','1',0}; /* *-bits, No parity, 1 stop bit */
char bin_name[1024];
int ex = 0;
FILE *Fptr = NULL;
do
{
if( argc <= 2 )
{
printf("Please feed the COM PORT number and the Application Image....!!!\n");
printf("Example: .\\etx_ota_app.exe 8 ..\\..\\Application\\Debug\\Blinky.bin");
ex = -1;
break;
}
//get the COM port Number
comport = atoi(argv[1]) -1;
strcpy(bin_name, argv[2]);
// ex = sizeof(ETX_OTA_HEADER_);
// printf("Opening COM%d...\n", ex );
printf("Opening COM%d...\n", comport+1 );
if( RS232_OpenComport(comport, bdrate, mode, 0) )
{
printf("Can not open comport\n");
ex = -1;
break;
}
//send OTA Start command
ex = send_ota_start(comport);
if( ex < 0 )
{
printf("send_ota_start Err\n");
break;
}
printf("Opening Binary file : %s\n", bin_name);
Fptr = fopen(bin_name,"rb");
if( Fptr == NULL )
{
printf("Can not open %s\n", bin_name);
ex = -1;
break;
}
fseek(Fptr, 0L, SEEK_END);
uint32_t app_size = ftell(Fptr);
fseek(Fptr, 0L, SEEK_SET);
printf("File size = %d\n", app_size);
//Send OTA Header
meta_info ota_info;
ota_info.package_size = app_size;
ota_info.package_crc = 0; //TODO: Add CRC
ex = send_ota_header( comport, &ota_info );
if( ex < 0 )
{
printf("send_ota_header Err\n");
break;
}
//read the full image
if(fread( APP_BIN, 1, app_size, Fptr ) != app_size )
{
printf("App/FW read Error\n");
ex = -1;
break;
}
for(uint32_t i = 0; i < app_size; i++)
{
printf("%d\r\n",APP_BIN[i]);
}
uint16_t size = 0;
for( uint32_t i = 0; i < app_size; )
{
if( ( app_size - i ) >= ETX_OTA_DATA_MAX_SIZE )
{
size = ETX_OTA_DATA_MAX_SIZE;
}
else
{
size = app_size - i;
}
//printf("%d\r\n", size);
//printf("[%d/%d]\r\n", i/ETX_OTA_DATA_MAX_SIZE, app_size/ETX_OTA_DATA_MAX_SIZE);
ex = send_ota_data( comport, &APP_BIN[i], size );
if( ex < 0 )
{
printf("send_ota_data Err [i=%d]\n", i);
break;
}
i += size;
}
if( ex < 0 )
{
break;
}
//send OTA END command
ex = send_ota_end(comport);
if( ex < 0 )
{
printf("send_ota_end Err\n");
break;
}
} while (false);
if(Fptr)
{
fclose(Fptr);
}
if( ex < 0 )
{
printf("OTA ERROR\n");
}
return(ex);
}if any one has faced the same issue can guide me.
thanking you
2022-10-11 5:21 AM
this one is original data when i used online .bin to hex converter
0x00, 0x00, 0x08, 0x24, 0xA1, 0x0D, 0x10, 0x08, 0xED, 0x0A, 0x10, 0x08, 0xF3, 0x0A, 0x10, 0x08, this is the data when fread function used
0x00, 0x00, 0x08, 0x24, 0x4D, 0x0C, 0x10, 0x08, 0x99, 0x09, 0x10, 0x08, 0x9F, 0x09, 0x10, 0x08,
2024-02-04 6:15 AM
Did you succeed? I am having a similiar task where i want to read the data contained in the .dat file. Can you provide your source code for this?
2024-02-04 11:18 AM
And what's the CORRECT data?
Say if you use a file viewer / manager, or hex editor on the PC with the original file.
Watch for parts of the system that handle CR/LF differently, want 7-bit data in transport path.
You should be able to CRC, SHA256 or MD5 the file in the application itself via standard test tools, and understand what's valid.
Watch for needs of flash to write in 4-byte or 8-byte units of alignment / granularity.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.