2024-02-02 1:07 AM
Need a help to work out the formula. I cant get my head around with this to work out. its polynomial with numerator and denominator. what is the formula for this. Thank you
FLOAT_TYPE num_coeff[] = {-2.42580348918581e2l, 4.43575581447635e2l, -8.6570608699616e2l, 7.34933695653457e2l, -7.02396810482965e1l};
FLOAT_TYPE den_coeff[] = {1.e0l, -8.87493143817912e-1l, 2.75291524634514e0l, -3.88521936154463e-1l, 9.08722079164108e-3l};
FLOAT_TYPE num_poly = num_coeff[sizeof(num_coeff) / sizeof(num_coeff[0]) - 1];
FLOAT_TYPE den_poly = den_coeff[sizeof(den_coeff) / sizeof(den_coeff[0]) - 1];
for (int i = (sizeof(num_coeff) / sizeof(num_coeff[0]) - 2); i >= 0; --i)
{
num_poly = num_poly * r + num_coeff[i];
}
for (int i = (sizeof(den_coeff) / sizeof(den_coeff[0]) - 2); i >= 0; --i)
{
den_poly = den_poly * r + den_coeff[i]; } return (num_poly / den_poly);
}
2024-02-02 7:21 AM - edited 2024-02-02 7:23 AM
num_poly(x) and den_poly(x) are each polynomials.
Result gives you num_poly(x) / den_poly(x).
Here, num_poly(x) = -2.42580348918581e2 + 4.43575581447635e2 * x - 8.6570608699616e2l * x^2 + 7.34933695653457e2 * x^3 - 7.02396810482965e1 * x^4
And den_poly(x) = 1.e0 - 8.87493143817912e-1 * x + 2.75291524634514e0 * x^2 - 3.88521936154463e-1 * x^3 + 9.08722079164108e-3l * x^4
2024-02-04 12:15 AM - edited 2024-02-04 12:30 AM
Thank you for the reply and formula. When I did the excel calculation on this I get a different answer using the above formula. But When I complie it I get different answer. Why is that
These are the numbers for derived formula.
| 1.000 |
| 1.038 |
| 1.057 |
| 1.067 |
| 1.077 |
| 1.081 |
| 1.085 |
| 1.089 |
| 1.092 |
| 1.096 |
| 1.100 |
| 1.104 |
| 1.108 |
| 1.112 |
| 1.116 |
| 1.193 |
| 1.289 |
| 1.385 |
2024-02-04 12:41 AM
float res2temp(float r)
{
int ni;
FLOAT_TYPE num_poly = num_coeff[sizeof(num_coeff) / sizeof(num_coeff[0]) - 1]; FLOAT_TYPE den_poly = den_coeff[sizeof(den_coeff) / sizeof(den_coeff[0]) - 1];
for (ni = (sizeof(num_coeff) / sizeof(num_coeff[0]) - 2); ni >= 0; --ni)
{
num_poly = num_poly * r + num_coeff[ni];
}
for (int i = (sizeof(den_coeff) / sizeof(den_coeff[0]) - 2); i >= 0; --i)
{
den_poly = den_poly * r + den_coeff[i];
}
return (num_poly / den_poly);
}
In this function I pass res2temp(6.e4f * adc_result / (1074547130368ll - (3ll * adc_result)))
The adc_result I putting are,
17909418.84,
18598931.46,
18944583.25,
19116513.67,
19288444.09,
19358290.82,
19426346.62,
19496193.35
,19564249.14
,19634095.87
,19702151.67
,19771998.4
,19840054.19
,19909900.92
,19977956.72
,21356981.97
,23081659
,24804545.09
its the same numbers when calculated adc_result, I mentioned above entering into excel but why excel gives different answer?
2024-02-04 1:02 AM - edited 2024-02-04 1:06 AM
Is it not like this , because I am not getting write answer
Num Poly = -70.2397+ 734.9337x-865.7061x^2 + 443.5756x^3 - 242.58x^4
Den Poly = 0.009087 - 0.38852x + 2.752915x^2-0.88749x^3 + x^4
2024-02-04 6:02 AM
@cjaya.2 wrote:Is it not like this , because I am not getting write answer
Num Poly = -70.2397+ 734.9337x-865.7061x^2 + 443.5756x^3 - 242.58x^4
Den Poly = 0.009087 - 0.38852x + 2.752915x^2-0.88749x^3 + x^4
I edited my response. Perhaps you are looking at the un-edited version. Here is what I wrote:
Here, num_poly(x) = -2.42580348918581e2 + 4.43575581447635e2 * x - 8.6570608699616e2l * x^2 + 7.34933695653457e2 * x^3 - 7.02396810482965e1 * x^4
And den_poly(x) = 1.e0 - 8.87493143817912e-1 * x + 2.75291524634514e0 * x^2 - 3.88521936154463e-1 * x^3 + 9.08722079164108e-3l * x^4
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.