STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DMA request generation on STM32H7

Hi!I am looking into the possibility on using LPTIM1 to trigger a DMA transfer with no CPU interrupt. This timer is chosen because it can be clocked directly by the HSE clock input. In the datasheet of STM32H7B3 (DS13139 - Rev 8) table 4, it states t...

HansPLJ by Associate III
  • 3430 Views
  • 4 replies
  • 3 kudos

Resolved! NUCLEO HSE from ST-LINK MCO is never ready

Newbie here!Setup:STM32CubeIDE 1.10.1Brand new NUCLEO-L476RG with MCO from ST_LINK MCU, no mods to the boardNew STM32 project using CubeMX 6.6.1, default mode for peripherals usedSystem Core -> RCC -> HSE = BYPASS Clock SourceClock configuration show...

gb2835_0-1707053291484.png gb2835_1-1707053460802.png
gb2835 by Associate II
  • 2656 Views
  • 2 replies
  • 1 kudos

STM32l4 + tinyusb + msc + sdmmc

Hi! I'm currently trying to mount my sdcard via MSC/SDMMC and tinyUSB. It worked fine with RAM, could read and write, but I probably do the commands wrong for SD Card. Mounting with FatFS works fine, but I cannot get it to display any device on my dr...

NW.2 by Associate II
  • 2235 Views
  • 0 replies
  • 0 kudos

DCMI and DMA to save multiple images on RAM

I'm currently evaluating the STM32U5 series to connect to a camera via DCMI and store video (i.e., multiple frames/images). For now, I would like to keep things simple and also learn how the DCMI and DMA workflow is like. So, I'll keep this forum pos...

Question about USB 2.0 HS support on discovery board

I need to do some testing with the STM32F767BIT6 MCU, to use the USB 2.0 HS USB peripheral. I can see it's used on this dev board ( https://uk.farnell.com/stmicroelectronics/nucleo-f767zi/dev-board-nucleo-32-mcu/dp/2546569 ) but the data sheet states...

Smashcat by Associate
  • 3257 Views
  • 4 replies
  • 1 kudos

printf() on NUCLEO-F767ZI board not working

I had written a function to support printf() using USART3 for NUCLEO-F767ZI board. Please check the code below, but I did not see the prints on the console in STM32CudeIDE. Please let me know what the issue can be. Do I need to do any changes on the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.