STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7B3I-DK - is it possible to use CAN and WiFI together?

The CAN connector on the board uses FDCAN1 on PA11, PA12 with PH8 being used to control the standby mode of the transceiver.To get the CAN interface working on the STM32H7B3I-DK I need to:Ensure that the STMOD+ connector is not used.Open SB22 and SB2...

CTapp.1 by Senior III
  • 1732 Views
  • 2 replies
  • 0 kudos

RTOS Survey

Bored Saturday, I was just curious who's using which RTOS:FreeRTOS (Hideous Hungarian HorroRTOS, where code is fugly and deficiencies are touted as features ;)Azure/ThreadX (can't wait to see how Microsoft poisons this one ;)RTX (any actual CubeMX su...

Resolved! Flash memory erase

I am using STM32L476RGT6. I am trying to read and write operation in the embedded flash memory. I am unable to erase the stored data in the embedded flash memory. I am following method to erase :FLASH_EraseInitTypeDef EraseInitStruct; HAL_FLASH_Unloc...

ADC triggered by timer running at half of expected speed

I am using NUCLEO-F756ZG board. Previously, I tried using ADC with timer trigger and it worked perfectly. Now, I tried to log the timer's pulse with another timer's input capture. It works but the captured timestamps seemed unusually slow. So, I disa...

rakib2023 by Associate III
  • 5199 Views
  • 2 replies
  • 0 kudos

Resolved! FLASH data cannot be read as expected using Memory Mapped Mode

I would like to read external FLASH data using Memory Mapped mode, which is a function of OctoSPI.The environment is as follows. Use Board : nucleo l4r5ziIDE : Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a.(Version: 9.3.0)FLASH : W25Q64JV C...

Myasu1_0-1704712676019.png
Myasu.1 by Senior
  • 9272 Views
  • 13 replies
  • 1 kudos

Resolved! STM32F100 PWM signal on PC6, setup question

Hi Firstly, sadly I can not change to HAL as I don't have time to port this all across right now for this project dealine. I am trying to setup a PWM signal on PC6 on the STM32F100, I am pretty sure I need to set it as an alternat function but I have...

TDuck.1 by Associate II
  • 5430 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.