STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H735G BSP_OSPI_NOR_Erase_Chip(0) not work

I have STM32H735G configured and worked with TouchGFX,. I have tihis configuration works:MX_OCTOSPI1_Init ->okayBSP_OSPI_NOR_Init(0, &ospi_nor_int)-> okayBSP_OSPI_NOR_EnableMemoryMappedMode(0)-> okay(post code)static void MX_OCTOSPI1_Init(void){ /* U...

Resolved! stm32h723 can not connect to the targer by SWD

I am not new in using STM32H7 products but in my last project I can not connect the target by ST_Link.I take care about power supply, pins to connect at GND or 3V3 and so on but the Link-Utility return this error:<<08:28:41 : ST-LINK SN : 44003200150...

Sacchy by Associate II
  • 6040 Views
  • 6 replies
  • 1 kudos

RTC Freezes in HAL_RTC_Init

Posted on June 07, 2017 at 11:16I am at my first time with RTC and I have some problems.I would like to configure rtc as a calendar.I would like to retrieve date and time after a certain event.I am following the RTC_Calendar example in the STM324xG_...

NUCLEO-U5A5ZJ-Q USB CDC ACM maximum speed using USBx

Hi,I am using NUCLEO-U5A5ZJ-Q board  to setup a USB VCP connection with PC. I am currently using the example project CDC-ACM, and getting a maximum speed of up to 4.4MBPS via the connection by increasing the Tx FIFO  size and Max Packet size in devic...

Kannan1 by Associate III
  • 8520 Views
  • 9 replies
  • 1 kudos

Resolved! STM32H747: PDM MIC voice/audio via network (VBAN) - for you

If you need an example, how to use PDM microphones (MICs) on STM32 MCU and how to bring the voice/sound via network to a host computer (PC) - here is my project:https://github.com/tjaekel/PortentaH7_VFR_CubeIDE Here is a YouTube video with a demonstr...

tjaekel by Lead
  • 2811 Views
  • 1 replies
  • 0 kudos

Resolved! Baud rate 230400

Hola, presento este error al visualizarr los bytes de salida por putty ▒``x▒▒▒▒▒▒▒`▒▒ ciclicamete, ya que es para un lidar ld06, connfiguro uart 2 velocidad de baudios 230400 la configuracion es  void SystemClock_Config(void) { RCC_OscInitTypeDef RC...

kzamudioq by Associate II
  • 7097 Views
  • 8 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.