2022-01-14 7:32 AM
I have STM32H735G configured and worked with TouchGFX,. I have tihis configuration works:
MX_OCTOSPI1_Init ->okay
BSP_OSPI_NOR_Init(0, &ospi_nor_int)-> okay
BSP_OSPI_NOR_EnableMemoryMappedMode(0)-> okay
(post code)
static void MX_OCTOSPI1_Init(void)
{
/* USER CODE BEGIN OCTOSPI1_Init 0 */
BSP_OSPI_NOR_Init_t ospi_nor_int;
/* USER CODE END OCTOSPI1_Init 0 */
OSPIM_CfgTypeDef sOspiManagerCfg = {0};
/* USER CODE BEGIN OCTOSPI1_Init 1 */
/* USER CODE END OCTOSPI1_Init 1 */
/* OCTOSPI1 parameter configuration*/
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThreshold = 4;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MACRONIX;
hospi1.Init.DeviceSize = 32;
hospi1.Init.ChipSelectHighTime = 2;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 1;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_DISABLE;
hospi1.Init.ChipSelectBoundary = 0;
hospi1.Init.ClkChipSelectHighTime = 0;
hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;
hospi1.Init.MaxTran = 0;
hospi1.Init.Refresh = 0;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.DQSPort = 1;
sOspiManagerCfg.NCSPort = 1;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_1_HIGH;
if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI1_Init 2 */
HAL_OSPI_DeInit(&hospi1);
ospi_nor_int.InterfaceMode = BSP_OSPI_NOR_OPI_MODE;
ospi_nor_int.TransferRate = BSP_OSPI_NOR_DTR_TRANSFER;
BSP_OSPI_NOR_DeInit(0);
if(BSP_OSPI_NOR_Init(0, &ospi_nor_int) != BSP_ERROR_NONE)
{
Error_Handler();
}
if(BSP_OSPI_NOR_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)
{
Error_Handler();
}
/* USER CODE END OCTOSPI1_Init 2 */
}
//end code
Then i try to use this functions, but nothigs works:
BSP_OSPI_NOR_Erase_Chip(0);
BSP_OSPI_NOR_Write(0, writebuf, 0, 100);
BSP_OSPI_NOR_Read(0, readbuffer, 0,100);
BSP_OSPI_NOR_ReadID(0,&myid);
Somebody can i help me please?
Solved! Go to Solution.
2022-01-17 6:26 AM
I solve this.
After BSP_OSPI_NOR_EnableMemoryMappedMode(0)
all other BSP command not work any more
2022-01-17 6:26 AM
I solve this.
After BSP_OSPI_NOR_EnableMemoryMappedMode(0)
all other BSP command not work any more
2024-02-23 3:30 AM
Hi,
im also facing similar issue,
how did you achieve the read and write erase operations on STM32H7 series with BSP APIs?
is there any application example available or any user manual available? to use the BSP OSPI NOR APIs? if yes, please attach here.
Thanks
2024-02-23 4:15 AM
The Reference Manual on the H7 side will usually provide a good outline of what the peripheral can do and the plumbing.
The OSPI memory device itself will also have a Data Sheet or Manual describing that ends expectations.
It would help to be specific about the memory part and how it interfaces with your board, to direct you the specific answers.
2024-02-23 4:24 AM - edited 2024-02-23 4:26 AM
Hi Tesla,
Thanks for Immediate response.
Im using STM32H735G-DK kit,
mx25lm51245g is NOR flash is connected.
I was trying to bring up the memory with BSP API's, is it possible to give any examples upon BSP API's
i have already checked, available examples from git repo :STM32CubeH7/Projects/STM32H735G-DK/Examples/OSPI/OSPI_HyperRAM_MemoryMapped at 5975bffae9358bc2b2890a35a203d940a395efef · STMicroelectronics/STM32CubeH7 · GitHub
this has been provided upon the HAL OSPI API
But I wanted to use BSP APIs instead HAL OSPI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.