STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

about Execute in place using dual quad spi

What I want to do is XIP with DUAL QUAD SPI.The environment is as follows.Use Board : nucleo l4r5ziIDE : Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a.(Version: 9.3.0)FLASH : W25Q64JVThe connection diagram of the board and FLASH is shown be...

Myasu1_0-1708448593094.png Myasu1_0-1708697574834.png Myasu1_1-1708698042431.png Myasu1_2-1708698571213.png
Myasu.1 by Senior
  • 6793 Views
  • 9 replies
  • 1 kudos

tft RGB close pins

hello i wand to use stm32h7 series LQFP package to connect RGB888 display first time i try with this chip   the alternate pins is not close to each other.. and for optimal high speed pcb traces, it be nice this pins to be close or im mistaken and not...

Lios by Associate II
  • 771 Views
  • 0 replies
  • 0 kudos

Resolved! Where to find LwIP incoming payload data for webserver?

STM32CubeIDE Version: 1.12.0Build: 14980_20230301_1550 (UTC)I have a STM32F407 Discovery board running a web server.  I have a simple webpage with a single button that when clicked, displays a text message below the button. I had issues with the serv...

Resolved! Dual-Bank Code Execution and OTA (STM32L073RZ)

Hi dear experts,I want to know is there a way to only program Bank2 and run the firmware from it? I manage to program Bank2 and set the BFB2=1 but i cant get the firmware to run. Am i making a mistake by not programming the Bank1 at all? i should men...

mehdihfzp by Associate II
  • 3245 Views
  • 2 replies
  • 1 kudos

STM32L083 AES peripheral

Hi community!Currently, I am using a MCU STM32L083 and I am trying to implement a bootloader. The firmware to be updated is encrypted with a AES-128 algorithm. The firmware is encrypted one time with a unique key for each divice and a second time for...

Direct I/O access

Hello,I want to ask if there is a way to access the I/O pins directly.Insread of writing "HAL_GPIO_WritePin(GPIOC, led1_Pin, 1);"   write "led1_Pin=1"or instead of "if(HAL_GPIO_ReadPin (GPIOC, myinput_Pin))" write " if(myinput_Pin);) Thanks for any i...

Polizos by Associate
  • 2199 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.