STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there any problem when boot0 pin is floating?

Unfortunately, I wrongly designed the PCB board So, the boot0 pin is currently floating (no connectable evenif temporaliy because of BGA pin layout).I'm getting trouble with programming. So, I want to know whether the programming error is happening d...

KKIM.6 by Senior II
  • 6774 Views
  • 8 replies
  • 1 kudos

STM32H7 WWDG expires during Flash Erase

I have been stuck on a tricky little issue for some time now.Using an STM32H753, on a reasonably large and complex application, when trying to erase the upper flash bank, the watchdog expires resetting the chip!My suspicion is that the CPU is stallin...

ADunc.1 by Senior II
  • 4958 Views
  • 4 replies
  • 0 kudos

ADC differences at an STM32F071V8Tx

Hi, we use 12 ADC channels to measure temperatures in a smart home project. The system clock of the STM32F071V8Tx is configured at 48 MHz. Due to the slow temperature curve, we use the longest sampling time. We have taken a conversion table from a da...

albreco_0-1708966365820.png
albreco by Associate
  • 1556 Views
  • 1 replies
  • 0 kudos

EEProm library clean time

I was reading the documentation from: https://www.st.com/en/embedded-software/x-cube-eeprom.html#documentationabout the eeprom lib. Concerning the cleanup time, I don't follow where the number comes from. I am using an L4 and there was only one examp...

dsauter_0-1708650884906.png
dsauter by Associate
  • 2834 Views
  • 4 replies
  • 1 kudos

Resolved! ADC_HandleTypeDef* h & (h = &hadc1)

Hi I come across an ADC code as below, could anyone advise whats the meaning of pointer *h in the function argument and whats (h = &hadc1) do inside the callback function ?main(void){ HAL_ADC_Start_IT(&hadc1); ... while (1) { if (adc_valid ...

Resolved! TFT Screen Library in STM32CubeIDE.

Dear Experts,I have 4 inch RPI LCD 480x320 SPI based on the ILI9486 display driver. Like inside ArduinoIDE, there is a Library manager where we can find so many TFT-LCD libraries with STM32 board support, Is there a common place to find libraries for...

YashJ by Associate III
  • 15228 Views
  • 4 replies
  • 0 kudos

STM32H5 USART RXFIFO error handing

Hello,I am developing a serial communication driver using USART.I have enabled FIFO and RTO interrupt, to handle reception.TRM says that the received data is stored in the RXFIFO together with the corresponding flags and that PE, FE, NE bits in ISR r...

CTabo.1 by Senior
  • 2885 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.