2024-02-27 12:26 AM
Hi,
I am trying to configure the pin PC13 in my STM32F411 device as Input with Pull up option and it is connected to a rotary encoder. At initial bootup time, the pin is in toggle state and after that, it is set to 0. In the same project, I also configured the RTC. This PC13 pin has an alternate function as RTC_AMP1, RTC_OUT, and RTC_TS. Could you please explain the reason for this?
Thanks and Regards
Vrinda R
Solved! Go to Solution.
2024-02-27 1:31 AM
Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-27 1:31 AM
Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.