STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NTC-Temperature Sensor

I used STM32F072C8T6.ADC - IN0, IN1 set.An application that measures temperature with an NTC temperature sensor.​   ​PullUp resistance 10K was connected to Vdd (3.29V) and PA0, PA1..When the HAL_ADC_Start_DMA function is executed, the voltage of ADC ...

스크린샷 2024-02-26 214841.png
hwm by Associate
  • 4390 Views
  • 2 replies
  • 0 kudos

STM32F302R8 ADC injected configuration weirdness

I'm seeing strange behavior trying to write to the ADC1_JSQR register. This register controls the channel sequence and the trigger source of injected conversions. After enabling the ADC (ADEN=1), a write to bits 7:0 (JEXTEN, JEXTSEL & JL) locks out f...

tld by Associate
  • 1223 Views
  • 0 replies
  • 0 kudos

stm32F412.. disco -- Unable to get the sdcard working.

I've been testing ST chips and started with the STM32F411 using my own board for testing with the SD card, which I wasn't able to get working. Thinking it was my fault, I ordered the STM32F412 Discovery board and I can confirm that using the examples...

pumarada by Associate III
  • 14379 Views
  • 17 replies
  • 4 kudos

Resolved! Porting WICED sdk from STM32F423 to STM32U5A5

Good morning, I have to do a porting from a project developed on STM32F423 to an STM32U5A5The starting project used the wiced sdk, with the supported platform STM32F423.If I understand well, for STM32U5A the wiced sdk is deprecated, and it would be b...

CORDIC COS implementation

https://github.com/Sushmitabaga/CORDIC/tree/main  I  was trying to Enable CORDIC IN STM32G4 series  for  checking the time taken by normal cos function and cos CORDIC function.  But i found that both are taking almost the same time. which is not poss...

Sushmita by Associate II
  • 5993 Views
  • 9 replies
  • 2 kudos

Resolved! No activate option of timer in STM32CubeIDE CubeMX

Hello, I am working with "Mastering The STM32" book and faced with one problem: cannot find the option as in the book to activate any timer using CubeMX. I am using STM32 blue pill STM32F103C8T6. Why I can't find the activate option of timers?

Resolved! NUCLEO H743ZI2 MB1364E and MB1364C

Hello, I hope you are doing great.I have two NUCLEO H743ZI2, one of them is MB1364E, and the other one is MB1364C. They are totaly the same but there are little differences and I would like to find them and make them same, since I would like to use t...

Waking up from RTC on a STM32G030

Hi all,I'm struggling for days why my RTC wakeup doesn't work.The program is running FreeRTOS, but I want the uC in Lowpower Sleep for 3 minutes.So I set RTC on 1Hz, counter 180 and internal wakeup.Activated the EXTI RTC interrupt.But it immediately ...

WSpar.1 by Associate III
  • 3048 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.