STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Wake up vs Alert in RTC

Hi, could someone explain me what is the difference between wake up and alert in RTC?For example the UM1749 provides information about RTC Alarm functions (section 39.2.8) and wake-up functions (section 40.2.2)When should I use the wake-up and when t...

STM32F072RB SPI DMA issue

Hi Team,We are using STM32F072RB MCU with discover EVM boardWe are using STM32CubeIDEWe are using SPI1 and SPI2 as slave mode configuration Query: we observed that the FIFO full and overflow is happening @Spi slave while receiving the data stream @1M...

Connecting to STM32 on NUCLEO-G474RE over USB

I'm just getting started with the STM32, only got the NUCLEO-G474RE board yesterday.I need to communicate from a PC to the STM32 over USB.  Am I correct in assuming that the CN1 USB connector is only available for ST-LINK, and I need to attach a seco...

Resolved! CAN1 communication doesnt work on nucleo-l433rc-p

Hi I'm new in working with CAN-bus. My project involves two stm32 boards (both are nucleo-l433rc-p) and I want to get CAN-bus communication between them. The code is supposed to make a build in LED blink each time the blue button on the main nucleo b...

Mr4_0-1709590357897.png Mr4_1-1709590366849.png Mr4_2-1709590413932.png Mr4_3-1709590425372.png
Mr4 by Associate III
  • 3266 Views
  • 4 replies
  • 0 kudos

USB Host MTP/PTP to digital camera

Hello, I'm testing the STM3240G-eval with the USB host MTP. The goal is to retrieve the photo from a canon EOS 100.The camera uses PTP protocol.As the demonstration  code read .wav file, I wrote a wav file to the root of the SD card. The digital came...

PCu1 by Senior
  • 6692 Views
  • 7 replies
  • 0 kudos

Getting TXUNDERR while writing data to eMMC

Hello -> We are using a custom board with STM32H745 controller and 8GB eMMC communicated with sdmmc. -> getting SDMMC_FLAG_TXUNDERR bit after writing 64 bytes to eMMC. But i am giving 1k buffer array to write. -> eMMC initialization, reading logic bl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.