2024-03-06 3:54 AM
Hello,
I have created a bootloader application that jumps to main application at 0x08010000.
It works fine, except when I run in debug mode. In this case, the first execution runs correctly. If I push stop and restart button the application goes to STKERR.
I setted:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
RAM3 (xrw) : ORIGIN = 0x20040000, LENGTH = 384K
FLASH (rx) : ORIGIN = 0x08010000, LENGTH = 1984K
}
in STM32L4R9ZITX_FLASH.ld and STM32L4R9ZITX_RAM.ld.
In main application, I setted
SCB->VTOR = (uint32_t)0x08010000
as first instruction.
What's wrong?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.