STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-f401RE frequency measuring using timer

Hello, I am trying to create a simple frequency measuring device using 1 optical encoder and NUCLEO-F401RE board. I want to capture frequency (or period) of impulse, so I was thinking to use input capture mode and capture rising edge of impulses and ...

DSimp.1 by Associate III
  • 2917 Views
  • 2 replies
  • 0 kudos

Is there a way to do deadtime compensation

Dear all,I'm new to this forum, so apologies if I post this in the wrong category. I'm trying to find a way to implement a deadtime compensation mechanism using a STM32G4. I have a 3-level 3-phase VSI. The switching frequency is 50kHz, the deadtime i...

Not able to enable TIM4 interrupt in NUCLEO-F756ZG

Trying out a simple timer w/ interruptI am using the below code to enable interrupt However during debug when ever I go to NVIC_SetVector(....)orTIM4->CR1 |= TIM_CR1_CEN; ;//-> CEN=1;//Start Timer4 I get an error'Break at address "0x80009b0" with no ...

JJAYAR by Associate II
  • 1984 Views
  • 2 replies
  • 0 kudos

Resolved! Connecting eMMC to SDMMC1 on the STM32H7

Hi.I am using SDMMC1-eMMC(16GB), SDMMC2-SD Card connected on a custom board.Both eMMCs and SD-Cards use FatFS as their file system.Both work fine when used alone.However, if you use f_open or f_write on FatFS on eMMC, you sometimes get an error and t...

DMA.png NVIC.png SDMMC1_SET.png SDMMC2_SET.png

stm32 timer doesn't count

hi, i have a problem with my stm32 timer in counter mode, i connected it to a lcd screen, and put a pulse signal in pin PB0, and i wanted to count these pulses and show them on the lcd, but the pulse count is stuck at 0, can you help me with it pleas...

medraouf by Associate II
  • 5401 Views
  • 7 replies
  • 1 kudos

ADC watchdog to Wake up from Sleep or Stop mode - STM32G050

I'm working on some code to wake up from Sleep or Stop mode when a low ADC value happens.I found this post which gets me almost all the way there https://community.st.com/t5/stm32-mcus-products/what-is-the-process-to-use-the-adc-on-stm32f745-to-wake-...

Screenshot 2024-03-01 at 2.45.55 PM.png Screenshot 2024-03-01 at 2.46.01 PM.png Screenshot 2024-03-01 at 2.46.06 PM.png Screenshot 2024-03-01 at 2.46.13 PM.png
marchold by Associate II
  • 3950 Views
  • 2 replies
  • 0 kudos

STM32C031C6T6 Multi channel ADC not working

Hello All, I am working on a raw STM32C031C6T6 directly soldered on a breakout board and trying to make a multi channel interrupt based ADC working but the problem i am facing is all the adc's are giving me the same values even after setting the sepa...

IMG-20240302-WA0000.jpg IMG-20240302-WA0001.jpg IMG-20240302-WA0002.jpg
RChou.1 by Associate III
  • 5786 Views
  • 8 replies
  • 0 kudos

Why RGB888 displays as black and white only

I followed the example in article AN4861 where STM explains how to setup RGB565all is working fine but when I switch to RGB888 I get only white and blackI use the image converter LCD-Image-Converter-20161012 tool explained in the article   the previe...

pic4.png pic1.png pic2.png pic3.png
MNapi by Senior III
  • 2830 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.