STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Store data in internal flash without erasing whole page

Hi, I would like to know method and sample code storing data without erasing whole memory page. I do refer example FLASH_EraseProgram, but i have wrote program that almost finish up the flash memory, if i erase a page, a 2KB page, it will erase my co...

Hollis_K by Associate III
  • 3569 Views
  • 6 replies
  • 3 kudos

Failed to trigger STM32L431 USART1 bootloader via SW

Hi guys,I could set MCU into bootloader mode manually by using PH3/Boot0, but I can't get trigger bootloader via SW... I did check previous posts, but somehow it does not help.HW setup: I have dev board with STM32L431. It has USART1 (PA9, PA10) conne...

Lex by Associate III
  • 1948 Views
  • 3 replies
  • 0 kudos

Resolved! Not a genuine ST Device!

HiI would like to debug STM32F303RDT6 using a combination of Keil and ULINK2.When I start debugging on the target microcontroller (STM32F303RDT6), **Not a genuine ST Device! Abort connection** is output as shown below.We investigated the cause.I foun...

Ukazu by Associate III
  • 8960 Views
  • 10 replies
  • 6 kudos

LORA E5 grove module

Hello,I'm currently sending AT commands to the Grove LoRa E5 module from Seed Studio, when I send commands like "AT," there is no response from the module. I've connected the module to the USART of the STM32L476RG board. If anyone has encountered and...

ADC frequency limit for ADCxDC2 use in STM32F446 (AN4073)

AN4073 states that ADCxDC2 can be used only if ADC frequency is at least 30 MHz. I used it by mistake with ADC frequency 22.5 MHz. It seemed like it improved the precision by about 5 LSBs. The software worked just fine: no crashes, no funny misbehavi...

vvp by Associate II
  • 4010 Views
  • 6 replies
  • 2 kudos

No output PWM for slave TIM channel

The MCU used is STM32F103VET6. I want to use TIM3_CH1 (generating a PWM signal of 10kHz, 30% duty cycle) as the master input of TIM4_CH1. The TIM3 acts as the prescalar of TIM4 and thus making TIM4 to ouput a PWM signal of 200Hz and 60% duty cycle. T...

OW1TY2_0-1710063630371.png
OW1TY2 by Associate II
  • 1367 Views
  • 1 replies
  • 0 kudos

Pinout and Configuration functions disabled?

Trying to configure my project to use USART2. When I opened "System Core" and "Connectivity", I see that a bunch of options are disabled or have warning signs. I haven't been able to find out why or how to change them, and this isn't an issue I have ...

Screenshot 2024-03-10 at 16.39.36.png

STM32G0B0 USB Interrupt Error Issue

MCU---STM32G0B0CET6CUBEIDE Settingx-tal 16MHzUSB CLOCK---48MHzUSB_DRD_FS---Host_Only_FS,USB_HOST---Mass Storage Host Class,FATFS---USB DiskUSB Interrupt---Enable[Probrem]If you set it to the above mode and operate it, the USB is recognized only once ...

Kimjunho by Associate II
  • 1815 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F756VGH6 not generating PWM.

Hi, I am a beginner STM32 user. I am exploring the STMCube ecosystem and some simple functions my MCU can do. However, I stuck on generating PWM signal (I simply dont get any signal on the pin, tried few different pins), which based on some youtube S...

Vilius_0-1705825909751.png Vilius_1-1705825993797.png
Vilius by Associate III
  • 9476 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.