2024-03-10 10:59 AM
Hi guys,
I could set MCU into bootloader mode manually by using PH3/Boot0, but I can't get trigger bootloader via SW...
I did check previous posts, but somehow it does not help.
HW setup: I have dev board with STM32L431. It has USART1 (PA9, PA10) connected to CP2105, which connected to the linux pc.
So far I wonder about these points:
Relevant code:
void JumpToBootloader(void)
{
uint8_t i;
void (*SysMemBootJump)(void);
volatile uint32_t addr = 0x1FFF0000;
__disable_irq();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
HAL_RCC_DeInit();
for (i = 0; i < (sizeof(NVIC->ICER) / sizeof(NVIC->ICER[0])); i++) {
NVIC->ICER[i] = 0xFFFFFFFF;
NVIC->ICPR[i] = 0xFFFFFFFF;
}
__enable_irq();
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
__set_MSP(*(uint32_t *)addr);
SysMemBootJump();
}
2024-03-10 2:24 PM - edited 2024-03-10 2:25 PM
> I can't get trigger bootloader via SW
How do you know?
Did you single-step the code above, or tried to stop it while running?
> Is __HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH() step needed on STM32L4?
If if does what its name promises (I don't use Cube/HAL), then yes - you need to map the system memory to address 0, as that is what the hardware does when you activate the bootloader, and the bootloader expects it to be mapped there. You may also make sure that VTOR is set to the default value of 0. You may also want to reset all peripherals in RCC during that process - essentially, you want to undo everything your program did with the mcu's registers until this point.
JW
2024-03-10 4:09 PM - edited 2024-03-10 4:10 PM
@waclawek.jan wrote:> I can't get trigger bootloader via SW
How do you know?
I checked it by two different ways:
1. I see that after JumpToBootloader() is executed, MCU is restarted with normal boot printouts.
2. By using STM32CubeProgrammer and trying to open /dev/ttyUSB1, which fails (and works if manually set boot mode).
I also saw a note in 2606 that "Due to empty check mechanism present on this product, it is not possible to jump from user code to system bootloader." However, it was stated for STM32L0 and absent for STM32L4 MCUs. Still wonder if it could be the case..
∕Lex
2024-03-10 5:01 PM
You still can single-step the jump in debugger, preferrably in disasm view. That should reveal, what's happening.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.