STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U585CIU6 UART upload issue

I'm having trouble uploading to or even properly recognising the STM32U585CIU6 (brand new chip from Mouser) this chip properly in the STM32CubeProgrammer 2.4.0 and hoping someone can help.I'm connecting UART via a generic FTDI, that is known to work ...

AdiXen by Associate
  • 1706 Views
  • 2 replies
  • 0 kudos

About project making

I want to make a structured project for stm32 with cmake where I want to make A parent folder like Stm32f4 and in that folder there will be multiple projects like blink, adc, uart and also there will be necessary header and source file(Hal) which wil...

Asraful by Associate III
  • 805 Views
  • 0 replies
  • 0 kudos

UClinux on STM32F4 Discovery

Posted on February 23, 2014 at 13:44Hello,I want to port uClinux on my STM32F4 Discovery board.I followed this tutorial :http://www.st.com/st-web-ui/static/active/jp/resource/technical/document/application_note/CD00242717.pdfand I have successfully(...

amine by Associate II
  • 3135 Views
  • 4 replies
  • 0 kudos

The interface firmware FAILED to reset/halt the target MCU

 Hello, I just bought an stm32 Nucleo-H743ZI2 and I can't upload a program with CubeIDE because it doesn't detect the stlink. Searching for solutions on Google, it seems it could be a firmware issue, and with STlink utility I get the same error, 'can...

sprintf not working when ADC started

I'm trying to send ADC results over to a receiver via UART, but somewhy the program freezes on sprintf() IF I have called HAL_ADC_Start_DMA() before. If I call sprintf() before HAL_ADC_Start_DMA() it works fine. However, I need to call it after start...

JS8 by Senior
  • 5263 Views
  • 10 replies
  • 0 kudos

Resolved! SCKL frequency of SPI

Hello,I have set the BR bit in CR1 to 0 with the expectation of obtaining an 8MHz clock frequency. However, I am encountering an actual frequency of approximately 1.042MHz. Does anyone have an explanation for this issue, or should I consider implemen...

Resolved! STM32F042F6P7 (TSSPOP20 package): CAN availability on CubeMx

Using STM32CubeIDE (v1.14.0) with STM32F042F6P7 (TSSOP 20) to configure CAN pins on custom board. However the CAN peripheral is grayed-out when I open the IOC file in STM32CubeIDE. For pin assignments, PB8 is available for CAN rx but CAN tx is not sh...

hexdecimal number to send UART

Hi,I wanted to send hexadecimal numbers through UART. I am using STM32F405. Can it be done.If I am sending float number as 1.3456 string (text) to windows COM port to  english language windows application field. If for example regional settings being...

cjaya.2 by Associate II
  • 2367 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.