STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051 Internal comparator configuration

Hi,I am trying to configure the internal cooperators in the STM32F051 micro-controller, but in the .ioc file I am able to configure only one Comparator. I require three comparators for my application. Is it possible to configure multiple comparators ...

Aiswarya1 by Associate II
  • 1415 Views
  • 7 replies
  • 4 kudos

I2S clock soruce - internal MSI RC or external HSE ?

I am using I2S (SAI) on the STM32L433 nucleo board and using the internal MSI RC as the clock source.I also have a 32.768kHz LSE external crystral which I believe helps to make the MSI RC clock more accurate when used with PLL.Is the internal MSI RC ...

freeflyer_0-1766003498399.png freeflyer_2-1766003858857.png

Choosing Internal vs external Clock

I do a project with the newer STM32 G , C series and i am curious what are the benefits of external clock vs using the internal clock, because it will save cost and layout space ?

DJMicro by Associate
  • 1062 Views
  • 2 replies
  • 0 kudos

BiSS-C Encoder feedback on EVSPIN32G4

Hello, as in this post i'm linkingIs there a way to use absolute encoders/resolvers ... - STMicroelectronics Communityi need to use a Biss-c absoulte encoder for a servo drive application using BLDC motors with STSPIN32G4, we are testing using EVSPIN...

Resolved! Changing the pin connections on the STM32F407VET6

Hi.I have Uart pins (Rx/Tx) PA3 and PA2 on STM32F407VET6. Can these pins be changed to I2C (SDA SCL) in the program?Are the pins on STM32 that have been assigned a protocol (SPI/I2C/Uart) constant and cannot be changed or replaced?Thank you.

No_Name by Associate III
  • 1585 Views
  • 7 replies
  • 1 kudos

STM32F407 Option Byte 0xFF, bricked chip

Hi fellows,I have a custom board with STM32F407VGT6. The board was able to be programmed via the JTAG (4 wire JTAG interface; Boot pin is pulled low to ground and reset is connected to the JTAG interface (Nrset pin)) with a segger programmer - multip...

Ratschaka by Associate II
  • 1485 Views
  • 12 replies
  • 1 kudos

LPTIMER Counter for Delay in STOP2 mode not working

Hello,I have application which go to STOP2 mode once no LPUART/Modbus communication (Running at 32Khz LSI clock) is in progress.Using lptimer for silence timeout logic for UART data frame completion. The code sometimes cause delay during modbus commu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.