STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F437 option bytes programming hangs

Hi, On startup my STM32F437 application checks whether JTAG RDP level 1 protection is enabled.  If it is not enabled then it enables it, ending with a call to HAL_FLASH_OB_Launch(), which loads option bytes and resets MCU. This all works fine, except...

small form factor

in the following link they present STM32 ODE:https://www.st.com/content/st_com/en/support/learning/video-page.html?products=FM116%2CCL1620%2CSC959%2CSS1532%2CLN1847&featuredVideosReferer=true&count=200in the video of "Prototype and develop more quick...

Yaser_0-1710296863790.png Yaser_1-1710296945289.png
Yaser by Associate
  • 1306 Views
  • 1 replies
  • 0 kudos

Timer22 never reach IRQ

Hi everyone,It seems that I have a problem with my Timer 22 configuration, on my Microcontroller, STM32L031 I would like to stop it then restart them with a lower speed to go into sleep mode, except that my interrupt is never triggered.  Do you have ...

Resolved! Write to Flash only 64Bit

Hello,Can I only write to the flash with 64 bit variables, or also 32/16/8 bit?I just used this function for this: HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, activepageaddress + u32_Offset, u64_Data)I have an STM32L432 uC.I already found this ex...

Martin42 by Associate III
  • 3223 Views
  • 5 replies
  • 3 kudos

Resolved! USB DFU STM32G474

Hello,I'm using NUCLEO-G474RE kit with soldered USB on PINs:PA11 - USB Data minusPA12 - USB Data plusVIN - VBUSIn the User configuration I have:nSWBOOT = CheckednBOOT0 = CheckednBOOT1 = CheckedThere is programmed program with blinking LED so I know i...

jha92_1-1710772303832.png jha92_0-1710772182564.png
jha92 by Associate
  • 3147 Views
  • 3 replies
  • 0 kudos

Resolved! Possible Errata Corrige in RM0456 manual, peripheral clock gating register RCC_AHB3AMENR not exists

Paragraph 10.7.3 of RM0456 manual for STM32U575/585 microcontroller cites registers RCC_AHB3AMENR and RCC_APB3AMENR to configure autonomous peripheral clock gating during stop 2 mode.However, I didn't find any other reference of such registers in the...

Resolved! What is 'digbypass clock source'?

Hi,I started a design with STM32U5 series MCU. In the STM32CubeX's HSE settings, there is a new option "DIGBYPASS Clock Source'. What's the differences with the old 'bypass clock source'?Thanks.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.