STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HX711 Load cell with STM32 Doubt.

Hi,I'm trying to interface the HX711 load cell with an STM32 MCU. The resultant values are varying by a huge margin after every interval so please help. I'm, uploading my codeSo PA6 - GPIO Input - DOUT pinPB9 - GPIO Output - Pulldown - SCLK Pin#inclu...

Resolved! STM32F4 external loader erratic function parameter passing issue

This is my first time making and external loader for an SPI flash device. I followed the examples and documentation I was able to find. I was to get the project setup on Keil and ".stldr" file loaded onto ST-Link Utility & CubeProgrammer.Initially, I...

grams by Associate II
  • 3959 Views
  • 7 replies
  • 3 kudos

how to interface lvds 1920*720

DSI2HDMI display converter - SL-MIPI-LVDS-HDMI-CNV (somlabs.com)how can i interface lvds display of 10.3 inch 1920*720 resolution with stm32f769-disc0 board.,,is there above module can be used for lvds signaling..or should i do schematic for interfac...

mbed_engr by Associate II
  • 1761 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H733ZG BOOT0

BOOT0 Input equivalent circuit data cannot be found. Please let me know if you have any materials.

mon by Associate
  • 2273 Views
  • 4 replies
  • 0 kudos

STM32F429IGT6 LTDC with RGB888 (854x480) image

Hello everyone! The MCU used is STM32F429IGT6.Among the functions, we want to use LTDC.Currently external memory cannot be used.using internal flash memoryI am trying to use an RGB888 (854x480) 24bit image.However, this image has a total size of 1.2M...

Jdogk_2-1710831788476.png Jdogk_3-1710832290039.png
Jdogk by Associate III
  • 2702 Views
  • 2 replies
  • 0 kudos

Where does the automatically downloaded STM32CubeMX update go?

Posted on October 06, 2015 at 20:59I noticed that there was a new CubeMX version available 4.10.1.  The Cube SW downloaded it semi automatically but I can't find it. It was unzipped automatically but not installed. So where is it. I have a Windows 7...

LMI2 by Lead
  • 3221 Views
  • 9 replies
  • 0 kudos

Resolved! STM32U5A5: PB5 and PB15 - failing (for your errata sheet?)

Dear STM team,I am debugging the chip since hours and I think there is something wrong with the PB5 and PB15 pins:1. SPI1 with MOSI on PB5:I have configured SPI1 and want to get the SPI1_MOSI on PB5 (as mentioned as ALT5 in datasheet).I use a STM32U5...

tjaekel by Lead
  • 5055 Views
  • 8 replies
  • 2 kudos

Nucleo-64 7 bit serial

I am using the Nucleo-64 STM32L476 evaluation board and am connecting via the (USB) debug port. This connects to USART2. However, when I send 7 bit serial (from the PC) it appears to arrive as 8 bit serial  (USART2). Does the USB to Serial converter ...

DOrch.1 by Associate II
  • 2024 Views
  • 3 replies
  • 2 kudos

Resolved! ADC pot conversions not stable in STM32F103RCT6

I am using stm32f103rct6 controller board. I am not getting fixed ADC values for POT. I was used poll for conversion in ADC. Please attach code to get a fixed ADC value or else please address me for how to solve the problem.

Yeswanth by Associate II
  • 5789 Views
  • 10 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.