2024-03-19 6:02 AM
DSI2HDMI display converter - SL-MIPI-LVDS-HDMI-CNV (somlabs.com)
how can i interface lvds display of 10.3 inch 1920*720 resolution with stm32f769-disc0 board.,,is there above module can be used for lvds signaling..or should i do schematic for interface board like below image which is done for eva board..my display is innolux DJ103IA-03B.
I WILLBE THANKFULL IF ANYONE CLEARLY EXPLAIN, as this is important for our dedicated HW too.
regards
embed_engr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.