STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Communication between DSP and PC

I am working on a pathological voice assessor device, using the STM32H747-DISCO development board. Currently focusing on sending a signal from the DSP to PC - there is also a separate connection for debugging from my Macbook which is plugged in to th...

shanzehq by Associate II
  • 2685 Views
  • 3 replies
  • 0 kudos

Help setting up I2S microphone!

I am trying to receive audio data from an I2S microphone (https://www.adafruit.com/product/3421) using my STM32L476RG board and its Serial Audio Interface (SAI). I'm using cubeIDE and I have the SAI set up as in the pictures below, however I am not s...

wecox2020_0-1710870921467.png wecox2020_1-1710870961271.png

Resolved! Another encounter with possibly fake chips.

Hello there,I know this is an old debate but since we are into production of a device using STM32G030F6 chips, we wanted to make sure the cheapest options are used while keeping them "original".The minimum price for the aforementioned MCU on ST e-sto...

Marzi by Associate
  • 2587 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G0x series multiple GPIO Pin functions

Hi,  Can I control the level of a GPIO Pin in software, if the GPIO Pin is in an Alternative function mode ?  For example, I have an application where I switch a MOSFET in Software, but I would like to use the Hardware or internal Silicon, and Softwa...

Resolved! UART transmitter transmits wrong ascii value to my pc.

UART transmitter transmits wrong ascii value to my pc. what is the problem in my code..??I put a charecter in Data Register, but serial terminal show another ascii code.My IDE is KeiluVision5. the code is in below.....  #include<stdint.h>#include<std...

Can't exit sleep mode

Hello.Using "ITEMIS Create" I've designed this simple statechart diagram to figure out the working principles of sleep mode. The diagram is shown below:The program should work like this: Device boots up, starts a timer, that has a period of 2 seconds...

BuderBrodas_0-1710617515754.png

NUCLEO-H755ZI-Q and VL53L4CX

Hi there, I want to setup the NUCLEO-H755ZI-Q to run just the microcontroller alongside a VL53L4CX ToF Sensor, I am currently having troubles, can anyone help? I am having troubles configuring the controller and printing values as UART is not configu...

isaacjack by Associate II
  • 1503 Views
  • 2 replies
  • 2 kudos

What's a good way to waste a clock cycle in STM32F4?

In the thread https://community.st.com/t5/stm32-mcus-embedded-software/why-does-my-tx-only-software-3-mbaud-uart-sometimes-send-strange/td-p/218077/page/2 I learned that "DSB" is a good way to waste a clock cycle in STM32F769. Now, what's a good way ...

arnold_w by Senior II
  • 5552 Views
  • 5 replies
  • 4 kudos

Resolved! Ethernet and LWIP on STM32F769 Discovery Board configuration issue

Hello,UsingSTM32CubeIDE V1.14.1TGFX 4.23.1STM32F769I-Disco BoardI want to use the ETH port to communicate with other devices.The project was generated with TGFX. I configured ETH port in RM|| mode, configured LWIP with disabled DHCP and manual IP set...

ED2 by Associate
  • 2425 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.