2015-10-06 11:59 AM
I noticed that there was a new CubeMX version available 4.10.1. The Cube SW downloaded it semi automatically but I can't find it.
It was unzipped automatically but not installed. So where is it. I have a Windows 7 machine2015-10-07 2:48 AM
For me, every time, I did an automatic update of STM32CubeMX, it dis not work afterwards anymore (exe missing).
So I always download and install it manually.2015-10-07 4:41 AM
Hi guys,
After launching thedowload of the new version 4.10.1 within ''Check Update Manager'': 1-Close CubeMx 2-Click right on its shortcut 3-Click on ''Run as administrator'' Then, updates will be installed completely. -Shahrzad-2015-10-21 2:49 PM
Tonight I did exactly like it was told below. But nothing happened. Or is it very slow or something?
2015-10-21 3:46 PM
Do you have any AV software that might be interfering with normal operation of the computer?
2015-10-22 7:46 AM
Heh. I have an antivirus suite from F secure. But I think this machine works quite normally (for a Microsoft product that is). That was a joke, everything works, no freezes or other problems. I can install drivers and so on. And CCleaner and so on are able to update themselves (if I let them). But for the next update I will try taking off the AV suite for awhile.
2015-10-23 2:19 PM
I have also experience the same issue but have another issue as well.
I downloaded the latest STM32CubeMX installer directly (not as an update within STMCube) and ran the installer with Administrative permissions. I then attempted to start the application using ''Run as Administrator'' and received the message in the attachment. Clive - How do I resolve this? What have I missed in the installation?? Eric ________________ Attachments : STM32CubeMX_update_Issue.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtgU&d=%2Fa%2F0X0000000aVi%2F4VnVjEd..NikriA5cYu7A3c0BRohA2A0_mYMC0MSMsk&asPdf=false2015-10-23 4:37 PM
Not really my battle.
I guess I'd look at the ownership/rights for the directories in question, and if they in fact exist. Files that are running (.EXE/.DLL) can't be deleted if the system has them loaded. Be very sure there aren't multiple instances of the software running, double check in the Task Manager.2015-10-27 9:32 AM
Hi apperley.eric.001,
Make sure of your administrator rights in the STM32CubeMx folder. Maybe it is the cause of the problem.-Shahrzad-2024-03-19 2:59 AM
Really? This is all you have to give as an answer? I'm running this out of an Command Prompt in Administrator mode and I get this same message.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.