STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reg. USB HOST HID Class Keyboard Implementation

Hello,I have been using STM USB HOST HID class library to implement the USB keyboard on my STM32F429ZI custom board. I have been able to successfully enumerate the USB keyboard and getting the key pressed on the keyboard using the custom keyread() fu...

shefu by Associate II
  • 1493 Views
  • 1 replies
  • 0 kudos

NEED AN ADVICE FOR NEW PROJECT

Hello everyone.I have to create an arbitrary waveform generator via DAC starting from a lookup array of 32 elements at least with 10bit resolution. However, I must be able to reach frequencies of around 300Khz. I wonder, which evaluation board can I ...

AntoR by Associate III
  • 2600 Views
  • 4 replies
  • 0 kudos

Flashing throught the MIPI interface and STLINK v3set

Hey guys. I'm trying to learn how to use the stlink programmers and program a nucleo board, without the use of the onboard programmer.I've successfully flashed the board by using the MIPI10 interface and the stlink. The thing is that i we want to mak...

Memory Hard fault with string lib

Posted on September 02, 2016 at 15:29 Hi everyone, I have a question about an hard fault generated by a line of code. I'm working with a STM32F401RE and Atollic True Studio The line is : sprintf (str, ''PAIR %s\r'' ,BT_deviceTAB[0].BDADDR); ...

dauphin2 by Associate II
  • 3591 Views
  • 6 replies
  • 1 kudos

Problem With UDP Broadcast receive

I am using the STM32F107VCT6 controller. use STMcubeIDE.I write the code of the UDP Server. but when I change the IP, subnet, and Gateway using TCP and reset the device. I do not get Broadcast info or the udp_recv function not working.void udpServer_...

LWIP.PNG
GETANS by Associate II
  • 4943 Views
  • 7 replies
  • 1 kudos

Resolved! STM32H563 Revision Z Creates a HardFault in the UCPD Library.

With revision Z of the STM32H563VIT6, which looks to be an older revision of the MCU, we get a HardFault issue in the UCPD library. We noticed the issue with revision Z, but revision X is working as expected (see errata in attachments)! When connecti...

mathieuM_0-1711120814750.png mathieuM_1-1711120814752.png mathieuM_2-1711120814754.png mathieuM_3-1711120814756.png
mathieuM by Associate II
  • 4426 Views
  • 2 replies
  • 5 kudos

Resolved! STM32H7 SD Card maximum writing rate

Hi Everyone,I use SDMMC on my STM32H7 to write data on SD Card. I have several question :- for now I can't reach better rates than 12Mo/s writing, using 32Ko buffers and with the stm32 doing only that. Is that normal? I think I should reach the 25Mo/...

Resolved! ADC in conjustion with DMA

HiI am facing an odd problem with ADC in conjunction with DMA on STM32L151V8T-A. I can see that it measures all three channels. However, the result of each channel is stored in the first element of my results array (Result[3]). Every time that the ca...

Pejwaak by Associate III
  • 7605 Views
  • 16 replies
  • 1 kudos

STM32H7A3 DCMI does not capture data.

Hello everyone.I've got a problem running DCMI interface on STM32H7A3 MCU. I'm using NUCLEO-H7A3ZI devboard and OV7670 camera module. Installed the latest CubeIDE and generated code in builtin configurator. Actually I'm using Segger Embedded Studio f...

image.png image.png
Dmitriy_L by Associate II
  • 4598 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.