2024-03-23 10:28 PM
if (HAL_GPIO_ReadPin(USER_Btn_GPIO_Port, USER_Btn_Pin))
{
HAL_GPIO_WritePin(TIGGER_GPIO_Port, TIGGER_Pin, GPIO_PIN_SET);
HAL_ADC_Start_IT(&hadc1);
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1,(uint32_t*) pwmData1, 300);
HAL_GPIO_WritePin(TIGGER_GPIO_Port, TIGGER_Pin, GPIO_PIN_RESET);
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
digitalValue2 = (((HAL_ADC_GetValue(&hadc1)) * 3.3f) / 4095.0f);
HAL_ADC_Stop_IT(&hadc1);
if( (digitalValue2 >= 0.0) && (digitalValue2 < 1.0))
{
for (int j = 0; j <= 300; j++)
{
pwmData1[j] = 100;
pwmData1[299] = 0;
}
}
else if ((digitalValue2 >= 1.0) && (digitalValue2 < 2.0))
{
for (int j = 0; j <= 300; j++)
{
pwmData1[j] = 300;
pwmData1[299] = 0;
}
}
else if ((digitalValue2 >= 2.0) && (digitalValue2 < 3.4))
{
for (int j = 0; j <= 300; j++)
{
pwmData1[j] = 200;
pwmData1[299] = 0;
}
}
else
{
for (int j = 0; j <= 300; j++)
{
pwmData1[j] = 50;
pwmData1[299] = 0;
}
}
HAL_ADC_Start_IT(&hadc1);
}
i am using this function using PWM generate and ADC interrupt function
using this every time updating the width it is taking 2ms delay
2024-03-23 11:50 PM
Primary dont start stop ADC, secondary your for cycles is ugly. And for any type of two device data transfers you require sync it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.