STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer pwm complementary for BLDC

I trying to figure out, how i should set up the complementary channels to achieve the signals, shown in the picture.If i would activate them (tim_oc1n), they would have a pwm, like the normal channel (just inverted). So i think it is only possible to...

Tobe by Senior III
  • 1912 Views
  • 1 replies
  • 0 kudos

STM32U585 FLASH READ PROTECTION

Dear Sir.I am using stm32u585 , I tested the flash read protection mechanism using STM32uCubeProgrammer it works , The STM32uCubeProgrammer  can't  find the target ,However doing FOTA is working.Is it ireversibble ?. Any way to set the CPU to "normal...

DFU go command fail to execute the code

Hi,I am creating a windows application to program an STM32G070 MCU using its built-in bootloader (MCU is blank) using UART & hex file.Programing is completed successful but to start the program i currently need to reset the device physically, which i...

rcohe.1 by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

RAMECC RAMECC_MxFAR

Hi,I am using the RAMECC_ErrorCount example to understand the working.  /* Analyse all memory */ for(Count = 0; Count < (MEMORY_SIZE / INC_OFFSET); Count++) { CurrentData = *(__IO uint32_t *)(MEMORY_BASE + (Count * INC_OFFSET)); }  * @bri...

andy_long by Associate III
  • 2384 Views
  • 2 replies
  • 0 kudos

Can STM32F407VGT6U acts like STM32407VGT6?

I just bought STM32 Discovery Board with STM32F407VGT6U ICs, the thing is i use the stm32duino extension on arduino IDE, and on one laptop we can't upload it, on other laptop the Board can't send Serial data, previously i use the STM32F407VET6 series...

Resolved! STM32U5 and USB HS

Hi allI'm configuring STM32U5A5VJT to work with the USB HS crystaless. From the Cube it seems to be possibile to use one of the integrated oscillators as clock source for the USB HS but this is not mentioned in the datasheet.I'm afraid that it could ...

Resolved! Mixed interrupts in the vector table

Hello,I'm looking the vector table described in the Table 97 of the STM32G4 series reference manual, and it shows interrupts with different characteristics, such as TIM1_BRK/TIM15 and TIM6_DACUNDER, being allocated to the same address. This is very c...

macalon by Associate II
  • 1869 Views
  • 2 replies
  • 1 kudos

Resolved! NUCLEO-F412ZG CAN Configuration issue

I having trouble getting the correct CAN timing configured with default 96Mhz System Clock on the NUCLEO-F412ZG eval board. I need a 250kbit/s baud rate. Here is what I have so far. The system clock setup is below.  

JDOG_0-1712351780796.png JDOG_1-1712351954587.png
JDOG by Associate III
  • 2182 Views
  • 2 replies
  • 1 kudos

Resolved! ESD protection for 2 USB port connectors

Hello,I setup a USB virtual com port which I use for serial comm.  My design has 2 boards; a panel-board and main-board.  The main-board has an STM32F373 with a USB-C connector as well as ESD321DYAR diodes for DM and DP USB line protection.The main-b...

LMorr.3 by Senior II
  • 6148 Views
  • 8 replies
  • 4 kudos

ADC for battery voltage monitor

Hi,I am using a STM32L4ZIT6 MCU. I want to monitor 4.2V Lipo battery voltage on an ADC pin. I have experimented two approaches:First:I used a 332k - 820k divider in order to drain low queiescent current. This is an high impendance measurement, where ...

lukin by Associate III
  • 7021 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.