STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C Slave address

Hello everyone!I am making a project with STM32F072 MCU and I have 3 devices that need to be controlled via I2C: a DAC, an ADC and a current monitor that has an ADC integrated. I've made the connections and part choices so that I have 3 different 7-b...

AlexB99_0-1712499662677.png
AlexB99 by Associate II
  • 1582 Views
  • 1 replies
  • 1 kudos

program MCU via system rom bootloader and CANBUS STM32F2

hello :)I am trying to program my MCU via system ROM bootloader. I have read an3154-can-protocol-used-in-the-stm32-bootloader-stmicroelectronics reference manual &an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics. I wrote a C++ ...

ELIRANBM by Associate
  • 1207 Views
  • 0 replies
  • 0 kudos

Resolved! Timer 1 Hallsensor interface - No interrupt from external signal.

This is how i the GPIO for the timer:// Hallsensors (Tim1 capture) my_GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2; my_GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; my_GPIO_InitStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init(GPIOC, &my_GPIO_Init...

Tobe by Senior III
  • 1520 Views
  • 2 replies
  • 1 kudos

Resolved! How to set a nand flash with FMC?

Hi there,I want to try touchGFX on my homemade board with the STM32F429BIT6 and a band flash chip H27U1G8F2B.I initial the FMC NAND flash by following the code:and test the NAND flash as below:The LOG output is like this(the data value sometimes chan...

Junde_0-1711690830124.png Junde_1-1711690868363.png Junde_2-1711690975526.png
Junde by Senior III
  • 3557 Views
  • 3 replies
  • 1 kudos

Resolved! HAL_Delay() stopped working after touchGFX initial?

Hi there,I am trying a touchGFX demo on my homemade board with STM32H743IIT6.Everything is OK except the HAL_Delay() is not working after the MX_TouchGFX_Init().The following code works well: ... MX_GPIO_Init(); MX_FMC_Init(); MX_CRC_Init();...

Junde by Senior III
  • 2417 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.