STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Parsing Raw Data

Hello,I need to parse a raw data that I receive UART3 interface. Then, I will send to a PC to show results in serial monitor. Before implementing in the microcontroller, I tested my approach in a C compiler. A sample raw data in the buffer array and ...

AE104 by Senior
  • 7911 Views
  • 12 replies
  • 3 kudos

Resolved! Stm32H743 ADC 16bit Really ?

The cubemx example for ADC scan of internal channels for 743-eval shows the converted values being multiplied by 4.  So is it really 16 bit or 14?  I have verified the necessity of multiplying by 4 to get correct readings for VBat.  

Stm32f429igt6-ltdc-lvgl

DescriptionIam using stm32f429igt6 board for displaying an image using ltdc display. I have used lvgl library for displaying an image. For 16bit RGB565 format lvgl V7.4 worked well and good but i want V9.1 in which 24 RGB666 format is available. I ha...

[STM32H5] ADC clock configuration for different ADCs

Hi, I am using both ADC1 and ADC2 for my project. I want both the ADCs to be configured with different Prescalar . But by doing so I am observing ADC2 working with the ADC1 Prescalar. Why am I facing this issue? Is it possible to configure both the A...

Anusha by Associate
  • 2776 Views
  • 4 replies
  • 0 kudos

Resolved! Embedded bootloader and HAL

Dear all.I've implemented a M3 and M4 program ( drive a iLi display and 485 port) now I'm porting it to the H5 (H562RGTX).One of the latest issue I'm facing is the jump from bootloader to application. In M3/M4 i used only LL, and the jump has no prob...

TheRaprus by Associate III
  • 2970 Views
  • 3 replies
  • 1 kudos

Resolved! CAN and USB on STM32767ZiT6

Hello,I have a custom board based on STM32767ZIT6 and it has the three CAN peripherals and the USB designed. The goal is to translate the CAN message to USB directly without the need for a bridge but I am facing issues activating the USB and the thre...

WIF by Associate II
  • 9885 Views
  • 11 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.