2024-04-12 4:48 AM
2024-04-12 4:53 AM
Use memcpy() ?
Check startup_f4xx.s for code that copies statics and Linker scripts for symbols.
2024-04-12 5:05 AM
I develop my Mcu driver code for stm32fdiscovery board by using two functions Mcu_Init and Mcu_InitClock.
But when I try to flash my code, I didn't get the values of register there .
Can you help me out with this.
2024-04-12 8:50 AM
Can you buy me coffee?
With the GNU/GCC model you typically use the linker script (.LD) to stage RAM data in ROM so at startup you can copy it. Code in the startup.s source file uses the symbols to determine the location and size of this data, and then has the assembler equivalent to memcpy() to move from the ROM staging area to the RAM destination.
Perhaps look at some of ST's supplied examples, and some college level texts on linkers, compilers, and embedded programming.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.