cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f429igt6-ltdc-lvgl

utthamsingh
Associate

Description

Iam using stm32f429igt6 board for displaying an image using ltdc display. I have used lvgl library for displaying an image. For 16bit RGB565 format lvgl V7.4 worked well and good but i want V9.1 in which 24 RGB666 format is available. I have upgraded my lvgl to V9.1 but so many things have changed from 7.4 to 9.1. I followed official documentation of lvgl to display an image in RGB565 format but in newer version i couldn't able to display anything. So kindly look into my code and provide solution.

What MCU/Processor/Board and compiler are you using?

STM32f429igt6 and iam using LTDC for display

What LVGL version are you using?

V9.1

What do you want to achieve?

I want to display an image

What have you tried so far?

I have tried v7.4 which works perfectly but it doesn't supports RGB565 format so i have switched to v9.1 but i think i messed up with the porting but i didn't get any error while building nor during running. And the documentation was not clear.

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.