STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to get free memory on USB drive with FatFs?

Hello,I would like to get free memory on USB drive (64GB, FAT32) with FatFs library. Here is part of my code:  DWORD fre_clust, fre_sect; uint64_t free_memory; res_file = f_mount(&fs, "0:", 1); res_file = f_getfree("0:", &fre_clust, &fs); fre_sect =...

Ondrej1 by Associate II
  • 1799 Views
  • 1 replies
  • 0 kudos

Resolved! [STM32L476RG] Jump to Bootloader from Software.

Posted on April 19, 2017 at 09:27 Hello, I want to use DFU for update my program on the STM32L476RG. I use a personnal board. When I put BOOT0 to VCC, the Bootloader start and we can change the firmware but my system is on battery and I have n...

Handling UART receive

I'm looking into creating a splashscreen and handling the uart responses. How can I wait for the input without consistently sending the response messaging. I'm unsure how to handle responses from the uart receive line.  enum splashscreen_response_typ...

mm.51 by Associate II
  • 1624 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer Error: No STM32 target found!

I have a STM32F405RGT6 on a custom PCB and are using a ST-Link/V2 ISOL in my computer. A USB-Mini is conencted to the ST-Link and from the ST-Link I use RESET, SWCLK, SWIO and GND to my STM32. I have tried connecting to the ST-Link with the STM32Cube...

mathieusteketee_1-1713515915240.png mathieusteketee_2-1713515989028.png mathieusteketee_0-1713515888552.png mathieusteketee_3-1713516411253.png

Resolved! STM32H750XBHX - CANFD Callback problem

Hey, I have a problem with the callback for FDCAN1. I am sending frames through ucandevices converter but the callback for FIFO0 is not called. The frames are definitely arriving, I added a test FreeRTOS and a task to receive and send frames to CAN1 ...

sqwerize by Associate III
  • 10435 Views
  • 16 replies
  • 4 kudos

Resolved! Pin to pin compatible option against STM32F779NIH6

Hello,I am currently Using STM32F779NIH6 for one of our application prototypes. Currently the internal RAM size is 512KB and based on our evaluation, for certain peripherals we need a higher RAM size ( Atleast 2X or 3X). Can you suggest any Controlle...

SRoy by Associate II
  • 1378 Views
  • 1 replies
  • 0 kudos

STM32F103C8T6 UL/VDE

Parts:STM32F103C8T6.UL/VDE certification data, MCU self inspection data, and IEC60730 safety certification report.I need these, if possible, send me an email,Thanks!jiangzz@unibtter-ic.com.

ZJian.2 by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4 OSC Problem

Hi everyoneI'm currently using the NUCLEO-F429ZI development board. I'm planning to create a PCB using the STM32F429ZIT6, but I've encountered some questions during the planning stage.According to the datasheet, HSE_OSC is specified to provide 8MHz, ...

Scarlet by Associate III
  • 10973 Views
  • 20 replies
  • 16 kudos

Resolved! How to abort SPI Slave when Master requests for less bytes?

Hi,I have my master and slave applications running on NUCLEO-H563ZI Boards both of which normally receive/transmit  10 bytes of data in each SPI transfer. I use SPI in DMA mode.However, in one test case, master starts a SPI transaction for only 4 byt...

WCarey by Associate III
  • 4094 Views
  • 7 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.