2024-04-19 3:10 AM - edited 2024-04-19 4:27 AM
I'm looking into creating a splashscreen and handling the uart responses. How can I wait for the input without consistently sending the response messaging. I'm unsure how to handle responses from the uart receive line.
enum splashscreen_response_type
{
TEST_RESPONSE_VALID,
TEST_RESPONSE_INVALID,
TEST_RESPONSE_UNKNOWN,
TEST_RESPONSE_MAX
};
int bootup_disp()
{
int test_type_response = TEST_RESPONSE_UNKNOWN;
char input[100]; // Buffer to hold the user input
int processed_input;
int chosen_test;
int resp_buff[1];
HAL_UART_Transmit(&hlpuart1,(uint8_t*)"USER CHOICE TYPE 1 for test:", sizeof("USER CHOICE TYPE 1 for test:"), 500);
HAL_UART_Transmit(&hlpuart1,(uint8_t*)"TYPE USER CHOICE:", sizeof("TYPE USER CHOICE:"), 500);
do{
HAL_UART_Receive(&hlpuart1,splash_resp_buff, 1,500);
if(resp_buff == 1)
{
HAL_UART_Transmit(&hlpuart1,(uint8_t*)"CORRECT CHOICE", sizeof("CORRECT CHOICE"), 500);
test_type_response = TEST_RESPONSE_VALID);
}
else
{
HAL_UART_Transmit(&hlpuart1,(uint8_t*)"INCORRECT CHOICE", sizeof("INCORRECT CHOICE"), 500);
}
}
while (test_type_response != TEST_RESPONSE_VALID);*/
HAL_UART_Transmit(&hlpuart1,(uint8_t*)splash_resp_buff, sizeof(splash_resp_buff)-1, 500);
2024-04-19 3:52 AM
Your code accepts any input as valid and no user input as invalid. You should consider no user input as a NO-OP and not as a incorrect choice.
2024-04-19 4:17 AM - edited 2024-04-19 4:26 AM
What do you mean by NO-OP ? So are you saying I should accept no response as incorrect ? What would you recommend doing ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.