STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1KBU6,STM32G0B1KET6

Hi, I am Murali Selvam from India, I have a doubt, Can we interface the external Micro-SD card through below given MCU, You have any reference schematic kindly give me. Thank you. STM32G0B1KBU6,STM32G0B1KET6

murali by Associate III
  • 1269 Views
  • 1 replies
  • 0 kudos

STM32H7 PDR_ON signal

I don't understand the goal of pin PDR_ON.From STM32H7 reference manual: I don't understand what "the power on/off reset function can be disabled" means. The product does not go to reset state even if the voltage goes below PDR threshold ?

Gpeti_0-1714482401598.png
Gpeti by Senior II
  • 3260 Views
  • 1 replies
  • 2 kudos

Upload example code to STM32F407

Using CubeMX, selecting "Start My project from Example" I find 33 examples if I filter for the "STM32F407G-DISC1" Board. I would like to have a deeper understanding of the one named "Demonstrations" I select it and "Start my project in External IDE" ...

pcb by Associate II
  • 3477 Views
  • 3 replies
  • 1 kudos

TSL library stateIDs

Hello everybody,I am trying to work with STM32F042G6 with TSL library but have some issues I hope that I made some minor mistake but I think I tried everíthing.I can't get stable detection when touching.I tried to copy a sample project but it was jus...

STM32F407 Mcu clock setup

Hello sir, I have developed MCU clock setup using two functions Mcu_init and mcu_initclock in stm32f407 board. Now I want to develop Distribute PLL and get PLL status. Can you help me out. I have attached my mcu.c here for your convinience.#include "...

Resolved! [STM32F769 ]Error: Flash Download failed - ''Cortex-M7''

Hi all,   I used the same setting and the same software, keil uVision5. The only different is use my own board rather than EVB, STM32F769I-EVAL. BTW, I use my own board and STM32 ST-Link utility. Sometimes I can successfully go to debug mode, but som...

AlbertC by Associate
  • 2649 Views
  • 1 replies
  • 1 kudos

Resolved! Stuck in sleepmode

I tried using the sleep mode in STM32L053R8, it gets stuck in this condition. what is the reason. if((ulpbit != 0) && (vrefinbit != 0)){SET_BIT(PWR->CR, PWR_CR_ULP);}

hazin by Associate III
  • 1214 Views
  • 1 replies
  • 0 kudos

STM32G474VET3: comparator characteristics

Hi, The propagation delay and offset error mentioned below for integgrated comparator. Can it be changed at higher temperature at 125 Deg c. So what will drift in propagation delay and drifts of comparator value at higher temperature lets say at 125 ...

sag_0-1714463408307.png
sag by Associate III
  • 840 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.