STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C Interrupts

I want to know the difference of the below 4 cases. Why the results are not as expected. Stm32 board is an i2c master with speed of 400kbps and slave is software simulation using Aardvark Total Phase Control Software.uint8_t i2c_tra[10] = { 0x1, 0x2,...

USB DFU & FLASH_PROGRAM_TIME

HiI successfully got USB DFU bootloader running based on this video.But one question: why is FLASH_PROGRAM_TIME 50 ms?How is this value dervied? What is the minimum possible value?Thx.

MK..1 by Senior
  • 1068 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F769, generate a 2kHz clock on PC9.

Hi,I'd like to have a 2kHz clock source on PC9, I was wondering if I can use TIM3_CH4 or TIM8_CH4 to do it. May you please help me to figure out it? My question is how to generate a 2 kHz clock on PC9 if I would like to use TIM3_CH4 or TIM8_CH4? Howe...

AlbertC by Associate
  • 1607 Views
  • 2 replies
  • 1 kudos

STM32 microsecond delay function with polling method

Hi,I am using stm32f0. I try to microsecond delay function. But, I observe that TIMx->CNT not increasing.I probably mistake on configutration function. But I could not solved. In 29 line, UF flag not to be setHere is my code;  void ledconfig(){ GP...

hazall by Associate III
  • 2138 Views
  • 3 replies
  • 1 kudos

Resolved! How to debug Stm32H755 Cm4 Core to get SPI clock running.

Hey Everyone,  I am having an issue with the stm32h755 dual debugging. Im trying to run cm4 by itself without cm7. But the issue im having is, whenever I reset the MCU and check the SPI lines, I see a clock running. When I debug just cm4, I do not se...

ACand.3 by Associate III
  • 2839 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F446xC/E - Newbie - Help

Good morningI am a newbie about MCUs.I would like to begin with a STM32F446xC/E MCU and a led blinking small project.So, I need some help with basic topics.-Can I put the STM32F446xC/E on a breadboard?-Can I program the STM32F446xC/E with a Nucleo de...

FabioCC by Associate II
  • 3481 Views
  • 8 replies
  • 2 kudos

STM32f071RB PA1 Comparator

Hello!I'm using Comparator 1 in the STM32f071rbt6 uC. The Comp  is properly configured, and sends an interrupt once triggered on PA1 referenced to PA4(DAC_OUT_1).it happened that the PA1 GPIO accidentally was not configured. Yet the comparator functi...

tage by Associate
  • 1292 Views
  • 2 replies
  • 0 kudos

STM-Studio doesn't recognize Java during the installation

I am trying to install STM-Studio, and during the installation process, it tells me that I need to install JRE version 7 or later. I've installed JRE 10, (If I wanted to install JRE 7 I had to go through the archive and it asked me to create and acco...

Nick C by Associate
  • 4848 Views
  • 5 replies
  • 2 kudos

Resolved! CAN bus calculated data is wrong, preset data is right

Good day I am sending a CAN message from a STM32F042. The first two bytes are the value read from an ADC split into 2 bytes. Then just for testing I set 4 bytes to "F042" which is then a fixed value that i know its sending what I ask. The problem I h...

CAlbe.2 by Associate II
  • 4508 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.