STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using STM32 HRTIM to Transmit the Input Signal to the Output

Hi,I want to use STM32G474's HRTIM for my project.There is one input(A) and 2 output(B,C) signals.I need to check the input signals controls and then I want to transmit the 'A' signal as the output as the 'B' signal. It should be same as the A signal...

0693W00000YA2qgQAD.png
gunccc by Associate II
  • 1783 Views
  • 1 replies
  • 0 kudos

STM32G0B1 FDCAN and bit timing

Hi,I would like to use the FDCAN peripheral of the STM32G0B1, for CAN2.0B.Coming from the F0 CAN peripheral, I can understand most of the new peripheral easily.However, for the bit timing, per FDCAN specification, there are 2 bit times: the nominal (...

Kraal by Lead
  • 5072 Views
  • 7 replies
  • 1 kudos

STM32H750 issue switching system clock to PLL1

I'm trying to get the STM32H750 discovery board running at 400MHz with as little code as possible. (plain C with ST's startup file, cherry-picking structs and defines from CMSIS)As far as I can tell I do most of the things, ST's examples do before an...

Resolved! Nucleo F446RE power supply

Good morningI am about to receive a Nucleo F446RE board.I'd like to add a 5V power supply, not using only the USB power supply.Can I give the supply from an AC/DC converter (220V AC to 5V DC)?Can I connect it directly to the board?Do I need to connec...

FabioCC by Associate II
  • 2331 Views
  • 1 replies
  • 0 kudos

Encryption csv file

HelloMCU has SD card & USB in MSC Device mode. I am storing data on SD card in csv fatfs format. The data from SD card can be read on computer by making connecting with USB. Now I want to encrypt the data so only my GUI application software on comput...

Nico3 by Senior
  • 3234 Views
  • 5 replies
  • 0 kudos

Resolved! Failed to read ROM table via AP 3 - Failed to start GDB server

 @RomainR. @mƎALLEm  UPDATE 04/30/24:I no longer believe this is a debugger only problem. CM7 is always successful in flashing and debugging or running.The ST Link GDB Server cannot flash the CM4 in either debug or Release mode. Please see attached f...

rtalan_0-1714485192455.png rtalan_1-1714485224939.png rtalan_2-1714485272517.png rtalan_3-1714485325426.png
rtalan by Associate III
  • 5834 Views
  • 5 replies
  • 0 kudos

Resolved! Delete repository files STM32Cube

I urgently need to free up space on Windows and this folder weighs about 20gb.Obviously I plan to save all these files in a flash drive before deleting it, to avoid any kind of problem,But I ask you what is this folder, what files it contains and if ...

luke514_0-1714828657993.png
luke514 by Senior
  • 2374 Views
  • 1 replies
  • 2 kudos

STM32G431RB fdcan module library 1.5.2 is not working

I am using motor control library with FDCAN port but STM32G431RB library is not workiking.I can solve the problem with changing code STM32G431cb fdcan library. The method is not proper method for using cubemx. Please update G431RB fdcan library.

Resolved! stm32u5 start up time too long

Hello, ST expert CubeMX generated software framework is used for our STM32U595VJT6 based hardware design. It works well but for the low start up time. It takes almost 1 second between 3.3V is stable and the flag GPIO turns high in MX_GPIO_Init. Is th...

Yang Yang by Associate III
  • 3451 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.