STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 ADC can capture the maximum frequency of sine waves

The maximum sampling rate of STM32H743 ADC1 and ADC2 is 3.6MSPS. According to the aroma sampling principle, the maximum sine wave frequency that can be collected is 1.8MHz. I don't know if I understand it this way, right? I want to collect higher-fre...

hanqingze by Associate III
  • 2651 Views
  • 3 replies
  • 2 kudos

STM32F722 clock initialization error

Hi,I'm working on a project that uses STM32F722RE and I wanted to set the system clock to max value of 216 MHz using 12MHz external crystal as the input for the PLL. The problem is, if I set the SYSCLK and HCLK to 216 MHz, the code fails to initializ...

Roach by Associate II
  • 5920 Views
  • 11 replies
  • 0 kudos

Resolved! STM32G0C1RET6(ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8))

Hi,          (STM32G0C1RET6  for this part number ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8) FLASH 64-LQFP (10x10))two type of pin descriptions have mentioned in the datasheet, I confused which one I have to...

lqfp.png
murali by Associate III
  • 1247 Views
  • 1 replies
  • 0 kudos

Resolved! Ethernet configuration issue

HI STM team,I am using NUCLEO-F439ZI BOARD. I am new to this board. According to the basic configuration the ETH selection shows the warning symbol, reference based on the internet example, the ethernet configuration it does not show the PHY Address ...

Ramachandran1992_0-1714455846651.jpeg Ramachandran1992_1-1714456093524.png

Pin function Spreadsheet

Does ST provide an excel or CSV form of a pin functionality spreadsheet, to aid in assigning pin connections during development? This would be similar to Table 13 in the datasheet, but not in PDF form.

Stan0402 by Associate II
  • 11768 Views
  • 11 replies
  • 3 kudos

Resolved! STM32U599VIT6Q - Not able to flash through the JTAG pins

Hello,I am using STM32U599VIT6Q for my project and I am unable to flash the MCU. When I turn on the board it consumes 50mA. Also, I am not using SMPS so I have connected the pins (VDDSMPS, VDDLXSPS, VDD11, and VSSSMPS) to the GND. Whenever I try to r...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.