2024-05-06 12:12 AM
Hi,
(STM32G0C1RET6 for this part number ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8) FLASH 64-LQFP (10x10))
two type of pin descriptions have mentioned in the datasheet, I confused which one I have to take for "STM32G0C1RET6" this part and which pin I will for watchdog timer so kindly help me. Find the screenshot for your reference.
Solved! Go to Solution.
2024-05-06 12:22 AM
This is explained in section 4 of the data sheet:
The devices housed in 32-pin, 48-pin, and 64-pin packages come in two variants - “GP” and “N” (the latter with ordering code having N behind the temperature range digit).
Hope that answers your question?
Regards
/Peter
2024-05-06 12:22 AM
This is explained in section 4 of the data sheet:
The devices housed in 32-pin, 48-pin, and 64-pin packages come in two variants - “GP” and “N” (the latter with ordering code having N behind the temperature range digit).
Hope that answers your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.