STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI on STM32U575 (NUCLEO board)

I'm trying to get SPI1 working on an STM32U575 (NUCLEO board), starting from a base of existing working STM32F4 LL API code, but have failed.I am running this on a NUCLEO-U575ZI-Q board, so MOSI on PA7 (D11), MISO on PA6 (D12), SCLK on PA5(D13) and w...

Memory writing problem of STM32L452RE

Hello fellow seniors:I am still in the learning stage and currently use the part of writing to the memory (Flash Memory). I have encountered a problem and would like to ask for advice:From the picture (instruction manual) of [[Figure 1]], we can see ...

螢幕擷取畫面 2024-05-08 163233.png

STM32H747 (Portenta H7) and HardFault Crash Report

My project crashes after a random period when sending network traffic (one hour or longer working). I want to debug (but without a debugger connected or sitting there and waiting). So, I want to record some data, e.g. when the HardFault_Handler was c...

tjaekel by Lead
  • 1538 Views
  • 0 replies
  • 0 kudos

STM32F429II LTDC Image size error

Hello, I was controlling the LTDC image with STM32F429II (Flash 2MB, RAM 256 + 4KB) from ST.I think there is an error in memory allocation, so I leave a question.The compiler i use is IAR.Currently, we have implemented the RGB888 image as 1.22MB size...

Jdogk_0-1715230831448.png
Jdogk by Associate III
  • 1023 Views
  • 0 replies
  • 0 kudos

stm32 spin eval 3201 connection issue

After downloading the latest version of MC workbench required drivers and the latest firmware. I am still getting the following error in the IDE- "Connection Failed! No response, check communication cable, the power or the baudrate(set to 9600)". Ple...

Jayadeep by Associate
  • 647 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.