STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with Flash writing and USB Host

Hello everyone,I'm working on a project with the STM32F412VET6 and I'm having an issue with flash writing when USB Host is active.When USB Host is active and I attempt to write to flash, execution gets stuck at the FLASH_FlushCaches() function, speci...

SDall.11 by Associate III
  • 1311 Views
  • 1 replies
  • 1 kudos

Resolved! Failed to toggle a LED with STM32F429I-Disco1

Hello, My board is STM32F429I-Disco1, the LED pin is PG13 and PG14, and the pins are set to 1. (So, after I click the run button,the LEDs light up). After I write the code "HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_13);" and "HAL_Delay(500);" in the "while ...

DJ_YANG by Associate II
  • 2878 Views
  • 4 replies
  • 2 kudos

Resolved! STM32L4 Read Out Protection setup issues

Hi all,I'm having issues getting ROP Level 1 setup on an STM32L412.Below is the code which is run pretty soon after every reset.After ROP has been set, and the system reset, ROP always reads back as 0xAA which leads to a boot loop of this function be...

mwp by Senior
  • 4260 Views
  • 5 replies
  • 4 kudos

USB host or usb cdc or UART

In my graduation project, I'm utilizing the STM32H735_DK microcontroller to communicate with a GMSL (Generalized Memory Scalable Logic) device. Typically, these devices are configured using terminal programs like Putty or TeraTerm. Commands, such as ...

sana1_0-1715029002465.png sana1_1-1715029034646.png sana1_2-1715029194638.png sana1_3-1715029876065.png
sana1 by Associate III
  • 9886 Views
  • 18 replies
  • 2 kudos

STM32H747 and I2C bootloader

Hello,I'm designing an electronic board with STM32H747 microcontroller. This is my first time using a microcontroller with 2 cores.I would like to ask some questions about bootloaders:- how do I select bootloader over I2C (I2C1 on PB6/PB9 pins)?- at ...

SSerg.4 by Associate III
  • 5094 Views
  • 2 replies
  • 0 kudos

Debouncing using registers

Hello, first of all, thanks for all the previous help to everyone. I want to debounce my input, using registers, but I'm running into the issue of it "not working" I am surely missing something in the logic I am overlooking.here is my interruptvoid I...

Petrarka by Associate II
  • 4233 Views
  • 1 replies
  • 0 kudos

unable to flash NUCLEO-H7A3ZI-Q

Hi Team,we are facing issue with flashing NUCLEO-H7A3ZI-Q board.is any problem if we flash stm32h7a3zit6 code on stm32h7a3zit6q.can we give a suggestion ASAP

Resolved! USB configuration

Hi, I need to use USB in 2 modes:1. See SD card files interfaced to controller through computer via USB2. Transfer SD card files to "data storage device (USB stick)" via USBAny examples for same? Display menu should handle above operations. Since the...

GauravK by Senior
  • 1680 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.