Ask questions, find answers, and share insights on STM32 products and their technical features.
Hello,I have a small problem when using a custom delay function as follows : void delay_us(uint32_t delayus) { uint32_t start_count = __HAL_TIM_GET_COUNTER(&htim2); while ((__HAL_TIM_GET_COUNTER(&htim2) - start_count) < delayus) { } } The attac...
I want to take ADC data at 166ksps but I am getting after 2 second. Can anyone suggest How can I take ADC data and also perform calculation ? Please give some guidance. I am attaching my main.c file.
Posted on January 15, 2017 at 18:50Hallo, i use the HAL to program a little test software to transfer data via spi between two STM32 Nucleo boards.One board with a STM32L476 sends every 5 ms 74 bytes of data as a spi master with 625 kBit.Chip selec...
Hi team,Looking for functional safety complaint MCUs.Kindly Suggest SIL3 certified MCU's which would be helpful for designing.
Hi, We are using STM32F103 in our project. Established IPC communication over USART. We have almost finished our development. We kept our setup running for long, sometimes we found that IPC-USART communication getting stuck, IPC does not work until w...
Hi.I want to save and load data to flash memory. (STM32F373RC)And initialization code was generated through cubemx.All functions including SPI, I2C, and ADC were successfully tested.However, saving and loading data into flash memory failed.All functi...
Hello forum, I'm starting to develop a smart robotic system, I wanted to base the movement part on an STM32 micro-controller,We thought about basing our SLAM on a camera and a simple distance sensor (and an IMU of course) for the initial mapping. the...
Hello,I am attempting to generate a waveform with a period of 33ms. In-between each period, I need to toggle the timer output 5 times with a varying timescale. My initial thought is to do this using a timer in output compare mode and then update the ...
Hi I'm new to the STM32 series, I have a NUCLEO-F401RE and the X-NUCLEO-53L8A1. I am trying to edit the code from the X-CUBE-TOF1 SW package but run into the error below when compiling. Any ideas on how to resolve this issue? Log output file: C:\Use...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.