STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Manual Keyboard Detection

hi,USB keyboard working fine via HID and i need have small Manual Keyboard Detection  by pressing button . it's not compiling  if( HAL_GPIO_ReadPin(GPIOC, button_Pin)) { if(USBH_HID_GetDeviceType(USBH_HandleTypeDef *phost) == HID_KEYBOARD)...

MMARI.1 by Senior II
  • 2125 Views
  • 3 replies
  • 1 kudos

Resolved! BOOT_ADD0 and BOOT_ADD1 are programmed with values 0xFFFF

Hi,I am using an STM32F746IE controller and in some of them i don't see proper ST programmed values in address locations of BOOT_ADD0 (0x1FFF 0010) and BOOT_ADD1 (0x1FFF 0018). As per the reference manual i understand the ST programmed values in thes...

3b004d21-7006-4235-8414-87c52f055602.jpg

stm32f103 timer input capture

Hi,I am trying to read some square signal with timer input capture for both falling and rising edge times. When i start the code, the interrupt routine works once, even if there is no signal. I am using the code below for setup timer and interrupt ro...

er3481 by Senior
  • 4274 Views
  • 6 replies
  • 0 kudos

STM32F205RGTx to E220-400T22D LoRa Communication Issue

Hello everyone,I'm currently working on a project involving the STM32F205RGTx MCU and the E220-400T22D LoRa module. I'm trying to send the command "C0 04 01 09" from my STM32 to the LoRa module, but it seems that the command isn't being recognized co...

Resolved! How to Configure multiple FD CAN RX_BUFFER ?

Hello,I configured my FD CAN on NUCLEO STM32H53 with the function as below. I want to have two RX Buffers to receive 2 specific CAN IDs. However, when I checked RX_BUFFER0 with if (HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER0) > 0...

ANguy.5 by Associate II
  • 4183 Views
  • 3 replies
  • 1 kudos

First test with "Blinking Led", but error message

Hello to everyoneI have connected a NUCLEO F446RE board, and I was following the tutorial "Step 2, Blinking LED" In the end, after launching the Debug, I receive the following error message.What does it mean? How can I solve?Tanks to anyone who will ...

FabioCC by Associate II
  • 2572 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer USB connect stalls at “IAP”

Hi there, folks. I hope someone familiar with this product can help me. I am trying to update the firmware in a Malahit DSP2 radio receiver that is powered by an STM32H743 MCU. I am following the manufacturer’s procedure, which utilizes STM32CubeProg...

JMora by Associate II
  • 2184 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.