2024-05-13 1:49 AM
Hello,
I have a small problem when using a custom delay function as follows :
void delay_us(uint32_t delayus) {
uint32_t start_count = __HAL_TIM_GET_COUNTER(&htim2);
while ((__HAL_TIM_GET_COUNTER(&htim2) - start_count) < delayus) {
}
}
The attached image shows the configuration of timer 2.
This delay function should allow me to generate short pulses. except that sometimes it does and sometimes nothing happens when I use it. I don't know what the problem is. Could you please help me?
Solved! Go to Solution.
2024-05-13 7:12 AM
Interrupt can be a reason for longer delay, or hal funtion do something
2024-05-13 2:11 AM
Hi,
you should not use some HAL lib calls , if you expect "us" timing, HAL might need 1 us itself .
And why on 32 bit counter ? need more than 60ms delay ? then use HAL_delay () .
I would try : (on TIM3)
void delay_us(uint32_t delayus)
{
TIM3->CNT = 0x0000 ; // start_count
while ((TIM3->CNT) < delayus) { };
}
2024-05-13 2:13 AM
Default promotion to INT.
2024-05-13 4:23 AM
the 32 bit counter was in the tutorial I followed on youtube.
why timer 3 and not timer 2?
2024-05-13 4:25 AM
I'm starting out in stm32 and unfortunately I don't understand what you're trying to point out. Could you be clearer? Please.
2024-05-13 4:37 AM
@LadyMt wrote:the tutorial I followed on youtube.
Please give a link to that tutorial
@LadyMt wrote:sometimes it does and sometimes nothing happens when I use it.
What do you mean by, "nothing happens"?
2024-05-13 4:44 AM
If I try what you suggest, I get stuck in the while loop.
Would you know why?
2024-05-13 4:47 AM
AGAIN propotion to int
Test your conditions
2024-05-13 5:04 AM - edited 2024-05-13 5:06 AM
@Andrew Neil wrote:
@LadyMt wrote:the tutorial I followed on youtube.
Please give a link to that tutorial
I can't find the video exactly. But I can show you another similar video that I also watched. : How to create delay in nano/micro seconds using timers in stm32 (youtube.com)
@LadyMt wrote:sometimes it does and sometimes nothing happens when I use it.
What do you mean by, "nothing happens"?
- There is no delay?
- Your system hangs?
- other ... ?
What I mean by "nothing happens" is that there are no delays.
I check this on an oscilloscope.
2024-05-13 5:57 AM
Did you start the timer , before using it ?
HAL_TIM_Base_Start(&htim3);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.