2026-01-11 2:38 AM
Hello
Im developing a CAN Bus node and with space constrains, so i ve looked in stm32 products and a qnf32 packages looked perfect for example stm32G0B1 has FDCAN.
The problem...These QFN32 dont expose HSE pins. I just can use HSI with 16 MHz +- 1% wich is not reliable for FDCAN, especially for industrial applications with many nodes.
I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.
Im i missing some thing here?
At are my alternatives? I now that QFN48 hás HSE, but i dont need só much io and the packages is bigger.
Help here
Solved! Go to Solution.
2026-01-11 6:41 AM
> I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.
> Im i missing some thing here?
PC14 can be used as OSC_IN in HSE bypass mode and fed with a clock signal. Use a TCXO rather than a crystal.
2026-01-11 6:41 AM
> I dont understand why the mcu hás 2 FDCAN peripherals if theres no reliable clock to Run them.
> Im i missing some thing here?
PC14 can be used as OSC_IN in HSE bypass mode and fed with a clock signal. Use a TCXO rather than a crystal.
2026-01-11 9:25 AM
Thank you TDK.
Never did that bypass and never used an TCXO. I'm civil engineer...
Do you have a schematic on how to connect a TCXO to the stm32 MCU with 32 pins? Do I need to connect something to OSC_EN pin?
Thanks a lot
2026-01-11 10:55 AM
A TXCO outputs a clock as a square wave. Connect the output to the OSC_IN pin. That's it. OSC_EN is not needed.
2026-01-11 11:06 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.